2008-06-12 1:20 AM
Reset at startup?
2011-05-17 3:36 AM
Hi
What should I do to get the stm32 to reset at startup? As it is right now, I have to push the ''reset'' button every time I have programed it, before the program starts executing. -Boelskov2011-05-17 3:36 AM
I managed to get it to restart after have programed it, by setting an option in uVision.
But it still do not start if I power it off and on again? Do I have to modify the startup-code? -Boelskov2011-05-17 3:36 AM
I found out that it depends on the powersupply. So it is probarbly because my powersupply is off an older date.
I think it has to be fixed in the software using the watchdog. -Boelskov