cancel
Showing results for 
Search instead for 
Did you mean: 

Rename project and also directory in STM32CubeIDE

chriskuku
Senior III

When renaming a project in the project tree view it seems one can rename the project itself but not the directory it initially had been created in.

I have a project "myfirst1", renamed it to "myfirst" with all references. In the treeview one can see that it has been renamed, but there is still marked like:

myfirst (in myfirst1)

Trying to rename myfirst1 to myfirst behind the curtain leads to things getting messed up.

How can I achieve this cleanly, so that "in myfirst1" disappears and the project is located in directory "first" in the filesystem?

10 REPLIES 10

This solution is kind of partial for me, doing this a new folder structure is created with the old names and creates a new .metadata.