cancel
Showing results for 
Search instead for 
Did you mean: 

reg addr's for GTZC_TZSC_MPCWMxANSR GTZC_TZSC_MPCWMxBNSR

Hedley
Associate III

The doc and SVD file don't have a reg at offset 0x44 (GTZC_TZSC_MPCWM3BNSR).

Since GTZC_TZSC_MPCWM3ANSR @0x40 exists, via symmetry I would expect B also at 0x44.

The doc does say this:

GTZC_TZSC external memory x non-secure watermark register 1

(GTZC_TZSC_MPCWMxANSR)

Address offset: 0x030 + 0x008 * (x-1), (x = 1 to 3)

and

GTZC_TZSC external memory x non-secure watermark register 2

(GTZC_TZSC_MPCWMxBNSR)

Address offset: 0x034 + 0x008 * (x-1), (x = 1 to 2)

In the debugger... it looks like its there... Here I set x=(1..3) for A&B

(gdb) set *0x50032430=0x11223344

(gdb) set *0x50032434=0x55667788

(gdb) set *0x50032438=0x44332211

(gdb) set *0x5003243c=0x88776655

(gdb) set *0x50032440=0xaabbccdd

(gdb) set *0x50032444=0xffeeddcc

(gdb) x/32x 0x50032400

0x50032400: 0x00000000 0x00000000 0x00000000 0x00000000

0x50032410: 0x00000000 0x00000000 0x00000000 0x00000000

0x50032420: 0x00000000 0x00000000 0x00000000 0x00000000

0x50032430: 0x01220344 0x00780788 0x04330211 0x01ab0655

0x50032440: 0x032304dd 0x023405cc 0x00000000 0x00000000

0x50032450: 0x00000000 0x00000000 0x00000000 0x00000000

0x50032460: 0x00000000 0x00000000 0x00000000 0x00000000

0x50032470: 0x00000000 0x00000000 0x00000000 0x00000000

tnx

Hedley

3 REPLIES 3
Imen Ezzine
ST Employee

Hi Hedley,

Can you please tell me the version of SVD file you are using for stm32L5?

Thank you,

-Imen

Hedley
Associate III

Hi Imen,

​

1.1

​

Tnx

​

Hedley​

Imen Ezzine
ST Employee

Hi Hedley,

I did verify and today we have a more advansed version (v1.4) for the STM32L5 svd files with more fixes if you are interested.

Nevertheless regarding the point you raised, I can see your confusing about expecting via symmetry a B register at 0x44 like for GTZC_TZSC_MPCWM3ANSR.

In our SVD deliveries we have to be aligned with RM (RM0438) which according to description GTZC_TZSC is limited at @0x40.

I am going to raise this point internally basing on your Debug observation and hopefully come back to you soon with an answer.

Thank you for your feedbacks!

-Imen