2018-02-28 3:55 AM
I have a few misunderstandings about DMA, so I need some help.
I setup DMA to copy from GPIO IDR (without inc) to sram (with inc), it triggered from Timer (Free Running, Overflow event).
In the case of algorithm like following:
1. DMA setup
2. Timer Start
3. Infinite Loop
4. Breakpoint in DMA Interrupt handler
All works fine, program jumps into interrupt handler, the sram buffer is filled up with some data from IDR. But when I change an
algorithm like that:
1.
DMA setup2. Timer Start
3.1. WFI (I'm using an assembler)
3.2. Infinite Loop
4.
Breakpoint in DMA Interrupt handler
The
interrupt
wakes core up, but the buffer is empty (not changed). DMA CNDTR register is 0 and there are no error flags. In Reference Manual I have this about WFI: 'CPU clock OFF, no effect on other clocks or analog clock sources', so, what did I miss? And how should I 'wait' for DMA interrupt without entering in checking loop?Another
misunderstanding
: I want to read least significant byte of IDR, so, I setup PSIZE = 16bits (as it said inReference Manual 'IDR
can be accessed in Word mode only'), MSIZE = 8bits (like inTable 76 in
Reference Manual). But sram is filled with halfwords anyway (doesn't matter what values of PSIZE (16bits/8bits) and MSIZE (16bits/8bits) are).
And some stupid misunderstanding
:
why can't I use source address of DMA in peripheral bit-band region as peripheral (to read specified GPIO bit)?
2018-03-01 3:14 PM
WFI refers to energy-saving modes. In this state, part of the periphery is turned off. Periphery is not reset, but the clock signal is removed. It can be controlled by the presence of a clock signal in a power saving mode, for this purpose there RCC registers.