cancel
Showing results for 
Search instead for 
Did you mean: 

reference schematic file for F429I Discovery board

James Anderson
Associate II
Posted on June 04, 2018 at 02:14

for most of the other boards I have looked at, the downloads section contains a 'schematic' package with the altium designer *.schdoc files for the board. The F429I discovery board schematic download only has the PDF file.

it is preferable to work from the reference design especially in this case for the SDRAM wiring which I'm not quite confident on. are these design files available anywhere?

#reference-design
2 REPLIES 2
Posted on June 04, 2018 at 03:21

The F429I-DISCO is the least useful and expandable design possible, poor for CAN, SDIO, ETHERNET, ADC etc

The EVAL boards have better SDRAM wiring/banking for code execution, but not fast or cached.

Some of the newer F4 parts have better options.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on June 05, 2018 at 00:00

Are you talking about the mcu itself or just about that board specifically?

I'm looking for a reference for wiring up an SDRAM to a 'Z' package STM32, though I likely will not use the F429ZI itself for the end design.