Question
Reading in ADC on STM32H753
I am trying to run a simple program that can read in data from a potentiometer through ADC. The pot is connected to PF10 or A5 on the nucleo board. My code is below:
When I run this it prints "Value is: 32767" once then stops. Because I am in continuous mode, it should keep printing a value. Also, even if I turn the pot and rerun the code, it always prints 32767 which makes me believe that value is not correct.
Any help is greatly appreciated! I am mostly unsure about the clock setup but it could be some other dumb mistake.
#include "stm32h7xx.h"
#include "printUSART.h"
#define ADC_ISR_LDORDY 0x1 << 12U
// ADC3_INP6 on PF10
// ADC3 on AHB4
/* Function prototypes */
int ADC3_Calibration(void);
void ADC3_Init(void);
void ADC3_IRQHandler(void);
int main(void){
USART3_Init();
// printf("\nCalibration factor is: %d", (int)ADC3_Calibration());
ADC3_Init();
ADC3->IER |= ADC_IER_EOCIE; // enable end of conversion interupts
NVIC_EnableIRQ(ADC3_IRQn); // enable on the NVIC
ADC3->PCSEL |= ADC_PCSEL_PCSEL_6; // preselect channel
ADC3->SQR1 |= ADC_SQR1_SQ1_1 | ADC_SQR1_SQ1_2; // select channel 6 as first in sequence
ADC3->SMPR1 |= ADC_SMPR1_SMP6_0 | ADC_SMPR1_SMP6_1 | ADC_SMPR1_SMP6_2; // max sampling speed
ADC3->CFGR |= ADC_CFGR_CONT; // continuous mode
ADC3->CR |= ADC_CR_ADSTART; // start conversions
while(1){
}
}
void ADC3_IRQHandler(void){
if(ADC3->ISR & ADC_ISR_EOC){ // if EOC flag is set
printf("\nValue is: %d", (int)ADC3->DR); // print value in data register
}
}
void ADC3_Init(void){
ADC3->CR &= ~ADC_CR_ADEN; // ensure that the ADC is off
RCC->AHB4ENR |= RCC_AHB4ENR_GPIOFEN; // enable clock for port F
RCC->AHB4ENR |= RCC_AHB4ENR_ADC3EN; // enable clock for ADC3
ADC3_COMMON->CCR |= ADC_CCR_CKMODE_0; // (25.4.3) choosing the clock source for ADC
GPIOF->MODER = GPIO_MODER_MODE10_0 | GPIO_MODER_MODE10_1; // setting PF10 as alternate function
ADC3->CR &= ~ADC_CR_DEEPPWD; // (25.4.6) takes ADC out of deep power down mode
ADC3->CR |= ADC_CR_ADVREGEN; // (25.4.6) enable the voltage regulator
while(!(ADC3->ISR & ADC_ISR_LDORDY)){} // (25.4.6) waits for reg to startup
/* Turning on the ADC (25.4.9) */
ADC3->ISR |= ADC_ISR_ADRDY; // clear the ADRDY bit
ADC3->CR |= ADC_CR_ADEN; // enable the ADC
while(!(ADC3->ISR & ADC_ISR_ADRDY)){} // wait for ADC to be ready
ADC3->CR &= ~ADC_CR_ADSTART;
}
int ADC3_Calibration(void){
/* Calibrating the ADC */
ADC3->CR &= ~ADC_CR_ADEN; // ensure that the ADC is off
ADC3->CR |= ADC_CR_ADCAL; // start calibration
while(ADC3->CR & ADC_CR_ADCAL){} // wait until ADCAL is 0 and cal is complete
printf("\nCalibration is complete");
return (int)ADC3->CALFACT;
}