cancel
Showing results for 
Search instead for 
Did you mean: 

Reading from Flash memory crashes the uC

Pejwaak
Associate III

Hi

We are facing problems when reading a data that is written to the flash using the following function?

Every time we write in reading the data the micro-controller crashes. Even if I want to see the content of the flash in that particular address using STM32Programmer, it throughs an error.

 

// Function to write structure to Flash void Flash_WriteStruct(uint32_t address, struct DeviceData* data) { FLASH_EraseInitTypeDef EraseInitStruct; uint32_t PageError = 0; // Erase the flash page (for example, page 2 at 0x08000200) EraseInitStruct.TypeErase = FLASH_TYPEERASE_SECTORS; EraseInitStruct.Banks = FLASH_BANK_1; // Address of page 2 EraseInitStruct.NbSectors = 1; EraseInitStruct.Sector = FLASH_SECTOR_2; // Number of pages to erase EraseInitStruct.VoltageRange = FLASH_VOLTAGE_RANGE_3; // Disable interrupts before starting the flash write __disable_irq(); SCB_DisableICache(); HAL_FLASH_Unlock(); if (HAL_FLASHEx_Erase(&EraseInitStruct, &PageError) != HAL_OK) { // Handle error __NOP(); } else { // Calculate the structure size in bytes uint16_t dataSize = sizeof(struct DeviceData); uint8_t buffer[32] = {0}; // Temporary buffer for 32-byte alignment for (uint16_t i = 0; i < dataSize; i+=32) { memset(buffer, 0xFF, 32); // Flash default value after erase memcpy(buffer, ((uint8_t*)data) + i, (dataSize - i > 32) ? 32 : (dataSize - i)); //uint8_t byte = *((uint8_t*)(data) + i); //HAL_FLASHEx_DATAEEPROM_Program(FLASH_TYPEPROGRAMDATA_BYTE, address + i, byte); // Write each byte of data to the EEPROM //HAL_FLASH_Program(FLASH_TYPEPROGRAM_FLASHWORD, address + i, byte); if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_FLASHWORD, address + i, (uint32_t)buffer) != HAL_OK) { // Handle programming error HAL_FLASH_Lock(); /* Enable instruction cache prior to internal cacheable memory update */ SCB_EnableICache(); // Re-enable interrupts after the write __enable_irq(); return; } } } HAL_FLASH_Lock(); // Lock the EEPROM /* Enable instruction cache prior to internal cacheable memory update */ SCB_EnableICache(); // Re-enable interrupts after the write __enable_irq(); } // Function to read structure from Flash void Flash_ReadStruct(uint32_t address, struct DeviceData* data) { // Calculate the structure size in bytes uint16_t dataSize = sizeof(struct DeviceData); for (uint16_t i = 0; i < dataSize; i++) { *((uint8_t*)(data) + i) = *(uint8_t*)(address + i); // Read each byte of data from the EEPROM } }
View more

 

 

 

3 REPLIES 3
TDK
Super User

So Flash_ReadStruct is producing a hardf fault? Set a breakpoint and show the values of the arguments you're using when you call it. Probably a bad pointer.

If you feel a post has answered your question, please click "Accept as Solution".
Pejwaak
Associate III

Hi

Thanks for you reply. I will do this. Can you please just explain what you meant by bad pointer?

I need to also mention that some time the data is read correctly and sometimes the read operation crashes the uC.

 

Regards,

Pej

Reading from an uninitialized or otherwise corrupted pointer which points to an invalid memory address will cause a hard fault.

If you feel a post has answered your question, please click "Accept as Solution".