cancel
Showing results for 
Search instead for 
Did you mean: 

Re: STM32H747I-DISCO: FDCAN1 TX not showing output in normal mode on PD1/PD0 (D3/D2)

prashanth1
Associate

Moved from this thread.

Thanks for the previous response — it helped me understand the configuration better.

 

Now I have a follow-up doubt:

 

In STM32CubeIDE, I can see multiple pin options for FDCAN1_RX and FDCAN1_TX in the pinout view. However, when I checked the STM32H747I-DISCO board, those selected pins (e.g., PB8, PB9, etc.) don’t seem to be accessible via any header pins or exposed GPIOs on the board.

 

So my question is:

Are there any accessible pins on the STM32H747I-DISCO board that I can actually use to connect FDCAN1 to an external CAN transceiver like the TJA1051T/3?

 

Would appreciate any guidance — especially if there's a known method to access these signals (e.g., via Arduino headers, PMOD, or solder points).

 

Thanks!

 

 

0 REPLIES 0