2016-10-21 2:12 PM
I have a few questions about the hardware debug support.
1) Is there a way for software to detect and active SWD connection ? 2) Any examples of using the debug monitor exception ?We're building some small data loggers and plan to use the SWD interface to configure and download data. The first question relates to using breakpoint instructions to signal the swd debugger -- if one is not connected, we want to skip the bkpt. (2) seems to offer a way for the debugger hardware to signal the device. I've had good luck using the st-util library to attach to a device and access the processor state -- even execute routines in the processor's memory. But, I'd like to do something a bit more principled.------- Edit ----I found the answer to most of my questions -- yes a running program can tell it a debugger is attached through theC_DEBUGEN
bit in the Debug Halting Control and Status Register DBCSR.
It looks like a custom ''debug monitor'' is the way to go for what I want to do. I can certain enter the debug monitor through polling. Still trying to understand how to thave the st-link trigger a debug monitor interrupt -- seems doable, but I haven't tried yet.