2010-12-12 08:12 PM
Question regarding ARM assembler's LDR instruction and address rounding
2011-05-17 05:18 AM
Also - a separate, but related question - the same page says that in the case of LDR
''The loaded data is rotated right by one, two or three bytes according to bits [1:0] of the address.'' What's up with that? EDIT: Okay, look at this: Say we got the same exact program as above, except there is a.byte 0x77
in the .data segment, just before the .word - giving us the following in memory (accounting for endianness): 77 BE BA FE CA Assume that the 77-byte is word aligned. Now, the address of var1 surely will be the same as before + 1. If we follow what the page I linked to said, we would now round this address down so that we read the 4 bytes 77 BE BA FE Note that I am talking about the first LDR here, I have not mixed in offsets yet. Now the page says that we ought to rotate this right, a set amount of bytes according to the two least significant bits. Since the address we requested (the BE byte) is word aligned + 1, we know that its two least significant bits must be 10 (little endian). So we are going to rotate our data 1 byte to the right. Doing this, accounting for endianness, I get BE BA FE 77 And as the page said, ''For a little-endian memory system, this causes the addressed byte to occupy the least significant byte of the register.'' But that is not what my debugger tells me. I get a nice 0xFEBABE77 in my register. So it seems like there has been no rotation... I am thoroughly confused.2011-05-17 05:18 AM
Unaligned memory accesses will typically cause the processor to fault in most ARM implementations.
So you shouldn't do 32-bit or 16-bit access from ODD addresses. And 32-bit access should have (A0=A1=0)2011-05-17 05:18 AM
Hmm according to the docs on keils website unaligned access is available - and on by default - on ARMv7. I use GNU's assembler, though, so there might be differences. Guess I'll just keep my data aligned.
2011-05-17 05:18 AM
In startup mode the mcus (STM32F103xx) support unaligned memory accesses, BUT they use much more cycles than aligned accesses (about factor 3-6). Accesses to flash can have higher factors because of waitstates!
In normal user mode unaligned access can fault. I think this can be disabled but with the same costs!2011-05-17 05:18 AM
I was in privileged mode, and it kind of worked, it just gave me slightly unexpected results...
It's not that I'm going to use unaligned memory access, I was just testing it 🙂 Knowledge is power, as they say.2011-05-17 05:18 AM
Cortex-M3 LDR is different to ARM7 LDR. There is no rotation on Cortex-M3.
For Cortex-M3 alignment behaviour see document ARM DDI 0405B section A3.2. (Maybe there is a later edition of this document).2011-05-17 05:18 AM
Are you sure? The document you mentioned didn't say anything about rounding at all, not that I could find at least. Still, it's a useful resource.
2011-05-17 05:18 AM
Section A6.7.42 shows the encodings for LDR (immediate).
What code bytes is your assembler generating?2011-05-17 05:18 AM
You need to include ldr r1,[r0,#3] in your assembly code.
After all, that is the instruction that was not doing what you expected.01 68 is ldr r1,[r0]