2017-09-24 3:31 AM
Hello,
I have a data in stored in quad SPI memory on device A, that I want to transmit to device B using SPI interface.
I was wondering if its possible to steam directly from quad-spi memory to SPI interface using DMA without buffering?
I have STM32L476 Discovery for testing
Thanks
Michael
2017-09-24 3:38 AM
Never tried, but I'd say yes, if the QSPI is in memory-mapped mode and the DMA is triggered from the SPI, it should behave as any other memory-to-SPI DMA. I wouldn't count on continuous SPI clock in case of SPI being master, though, and would consider timing issues should the SPI be slave.
JW
2017-09-25 6:17 AM
JW,
Thank you for your replay, its a good idea to use QSPI and memory mapped.
The SPI is slave, how can I evaluate the timing and check for issues?
Michael