2017-06-21 12:40 PM
System: SW4STM32
STMCubeMX
ST32F765
Custom board.
Hi!,
How can I mount a QSPIFlash to the FAT filing system?
The memory chip on the QSPI interface is a S25FL256.
In googling for this I came across user_diskio.c (from ST) that makes uses a QSPIFlash library, but I can't find this.
2017-06-21 2:38 PM
http://www.st.com/en/embedded-software/x-cube-extboot.html
The HAL contains some QSPI code also
2017-06-21 4:43 PM
You should perhaps query the guy that posted the user_diskio.c file you are using.
Look in the sources provided by the ST-LINK Utilities to build external loaders for ST boards using QSPI Flash