2014-11-27 4:51 AM
Hi,
i am trying to generate an Signal with 50 % duty cycle using PWM Mode 1 Timer 1 channel 1.Pls go through the code below.I can't generate any pulse at PE9 PE9 is used as timer 1 channel 1 PWM OP. Using HSE 8Mhz with PLL=HSE*9; SYSCLK=72Mhz. void Configure_Controller(void) { Reset_Clock_Control(); GPIO_Configuration(); Configure_Timer_1(); } void Reset_Clock_Control(void) { ErrorStatus HSEStartUpStatus; //To handle Error Status of HSE RCC_ClocksTypeDef RCC_Clocks_Attributes; RCC_DeInit(); // Reset the RCC clock configuration to the default reset state HSI ON,HSE & PLL OFF RCC_HSEConfig(RCC_HSE_ON); //Enable external clock 8Mhz HSEStartUpStatus = RCC_WaitForHSEStartUp();//Wait till HSE is ready and if Time out is reached exit if(HSEStartUpStatus==SUCCESS) //if HSE is stable { Exception_Object.HSE_Clock_Exception=0; FLASH_PrefetchBufferCmd(FLASH_PrefetchBuffer_Enable);//Enable Prefetch Buffer FLASH_SetLatency(FLASH_Latency_2); //Flash 2 wait state RCC_PLLConfig(RCC_PLLSource_HSE_Div1,RCC_PLLMul_9);// (HSE Clock*9)/1; RCC_PLLCmd(ENABLE); //Enable PLL with 72MHz while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET);//Wait untill PLL is ready RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK); //Select the PLL as system clock Source while(RCC_GetSYSCLKSource() != 0x08); //Wait untill PLL is used as system clock RCC_HCLKConfig(RCC_SYSCLK_Div1); //use HCLK/AHB =system clock/1; 72Mhz RCC_PCLK1Config(RCC_HCLK_Div2); //APB1 HCLk/2=36Mhz RCC_PCLK2Config(RCC_HCLK_Div1); //APB2 HCLk/1=72Mhz RCC_LSEConfig(RCC_LSE_OFF); //Disable LSE RCC_LSICmd(DISABLE); //Disable LSI RCC_GetClocksFreq(&RCC_Clocks_Attributes); //Get Present Clocks if((RCC_Clocks_Attributes.SYSCLK_Frequency==72000000)&&(RCC_Clocks_Attributes.HCLK_Frequency==72000000)&&(RCC_Clocks_Attributes.PCLK1_Frequency==36000000)&&(RCC_Clocks_Attributes.PCLK2_Frequency==72000000)) Exception_Object.Clocks_Exception=0; else Exception_Object.Clocks_Exception=1; RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOD | RCC_APB2Periph_TIM1 | RCC_APB2Periph_AFIO, ENABLE); //Port E & Timer 1 & AFIO RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4,ENABLE); } else { Exception_Object.HSE_Clock_Exception=1; RCC_HSICmd(ENABLE); //Enable } } /************************************************************************************************************************************************************* ****** Routine name:GPIO_Configuration ****** Formal Argument:None ****** Retur Type:None ****** Used to Intializse the Port Pins * PE^9: 10HZ Timer 1 Channel 1 with 50 % duty cycle **************************************************************************************************************************************************************/ void GPIO_Configuration(void) { GPIO_InitTypeDef GPIO_Configuration_Object; GPIO_DeInit(GPIOE); //Reset the GPIO Port E to default value GPIO_Configuration_Object.GPIO_Pin=GPIO_Pin_9; //Used for Generating 10 HZ signal through PWM_TIM1_CH1 GPIO_Configuration_Object.GPIO_Speed=GPIO_Speed_2MHz; GPIO_Configuration_Object.GPIO_Mode=GPIO_Mode_Out_PP; GPIO_Init(GPIOE, &GPIO_Configuration_Object); //Initialise the PORt with required setting GPIO_PinRemapConfig(GPIO_Remap_TIM1, ENABLE); // Configure peripheral I/O remapping } /************************************************************************************************************************************************************* ****** Routine name:Configure_Timer_1 ****** Formal Argument:None ****** Retur Type:None ****** Used to enable timer 1 channel 1 with 10 hz 50 % duty cycle **************************************************************************************************************************************************************/ void Configure_Timer_1(void) { TIM_OCInitTypeDef TIM_OCInitStructure={0}; TIM_TimeBaseInitTypeDef Timer_Struct_Object={0}; TIM_DeInit(TIM1); //Reset the Timer 1 Timer_Struct_Object.TIM_Period=50000; Timer_Struct_Object.TIM_Prescaler=144; Timer_Struct_Object.TIM_ClockDivision=TIM_CKD_DIV1; Timer_Struct_Object.TIM_CounterMode=TIM_CounterMode_Up; TIM_TimeBaseInit(TIM4, &Timer_Struct_Object); TIM_Cmd(TIM1, ENABLE); TIM_SelectOCxM(TIM4, TIM_Channel_1, TIM_OCMode_PWM1); TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = 250; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OC1Init(TIM1, &TIM_OCInitStructure); TIM_OC1PreloadConfig(TIM1, TIM_OCPreload_Enable); TIM_CtrlPWMOutputs(TIM1, ENABLE); }2014-11-27 6:08 AM
Bunch of TIM4 references still in there. TIM1 you'd also want to fully qualify all the OC structure fields, including the inverting output fields.