PWM not work by using TIM10_CH1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2013-09-03 11:22 PM
Posted on September 04, 2013 at 08:22
My platform's MCU is STM32f205.
I try to modify TIM10_PWMOutput example from STM32F2xx Standard Peripherals Firmware Library to generate one PWM signal by using TIM10_CH1function of pin PB8. But it doesn't work? Can somebody help me to fix this issue? please see the reference codes as below. int main(void) { /* TIM Configuration */ TIM_Config(); /* --------------------------------------------------------------------------- TIM10 Configuration: generate 1 PWM signal: In this example TIM10 input clock (TIM10CLK) is set to 2 * APB2 clock (PCLK2), since APB2 prescaler is different from 1. TIM10CLK = 2 * PCLK2 PCLK2 = HCLK / 2 => TIM10CLK = HCLK = SystemCoreClock To get TIM10 counter clock at 20 MHz, the prescaler is computed as follows: Prescaler = (TIM10CLK / TIM10 counter clock) - 1 Prescaler = (SystemCoreClock /20 MHz) - 1 To get TIM10 output clock at 30 KHz, the period (TIM10_ARR) is computed as follows: ARR = (TIM10 counter clock / TIM10 output clock) - 1 = 665 TIM10 Channel1 duty cycle = (TIM10_CCR1/ TIM10_ARR)* 100 = 50% Note: SystemCoreClock variable holds HCLK frequency and is defined in system_stm32f2xx.c file. Each time the core clock (HCLK) changes, user had to call SystemCoreClockUpdate() function to update SystemCoreClock variable value. Otherwise, any configuration based on this variable will be incorrect. --------------------------------------------------------------------------- */ /* Compute the prescaler value */ PrescalerValue = (uint16_t) (SystemCoreClock / 20000000) - 1; /* Time base configuration */ TIM_TimeBaseStructure.TIM_Period = 665; TIM_TimeBaseStructure.TIM_Prescaler = PrescalerValue; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM10, &TIM_TimeBaseStructure); /* PWM1 Mode configuration: Channel1 */ TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = CCR1_Val; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OC1Init(TIM10, &TIM_OCInitStructure); TIM_OC1PreloadConfig(TIM10, TIM_OCPreload_Enable); TIM_ARRPreloadConfig(TIM10, ENABLE); /* TIM10 enable counter */ TIM_Cmd(TIM10, ENABLE); while (1) {} } /** * @brief Configure the TIM10 Ouput Channels. * @param None * @retval None */ void TIM_Config(void) { GPIO_InitTypeDef GPIO_InitStructure; /* TIM10 clock enable */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM10, ENABLE); /* GPIOF clock enable */ //RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOF, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE); /* GPIOF Configuration: TIM10 CH1 (PF6) */ //GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 ; /* GPIOF Configuration: TIM10 CH1 (PB8) */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 ; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ; //GPIO_Init(GPIOF, &GPIO_InitStructure); GPIO_Init(GPIOB, &GPIO_InitStructure); /* Connect TIM pins to AF3 */ //GPIO_PinAFConfig(GPIOF, GPIO_PinSource6, GPIO_AF_TIM10); GPIO_PinAFConfig(GPIOB, GPIO_PinSource8, GPIO_AF_TIM10); } #pwm-stm32-tim10
Labels:
- Labels:
-
TIM
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2013-09-04 7:39 AM
Posted on September 04, 2013 at 16:39
The following worked for me on an F4, should be directly portable to an F2
// STM32 PWM (TIM10 30KHz PB8) STM32F4 Discovery - sourcer32@gmail.com
#include ''stm32f4_discovery.h''
/**************************************************************************************/
void RCC_Configuration(void)
{
/* --------------------------- System Clocks Configuration -----------------*/
/* TIM10 clock enable */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM10, ENABLE);
/* GPIOB clock enable */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);
}
/**************************************************************************************/
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/*-------------------------- GPIO Configuration ----------------------------*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_Init(GPIOB, &GPIO_InitStructure);
/* Connect TIM10 pins to AF */
GPIO_PinAFConfig(GPIOB, GPIO_PinSource8, GPIO_AF_TIM10);
}
/**************************************************************************************/
void TIM10_Configuration(void)
{
TIM_OCInitTypeDef TIM_OCInitStructure;
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
uint16_t Period;
Period = SystemCoreClock / 30000; // Accurate 30 KHz from 120 or 168 MHz
/* Time base configuration */
TIM_TimeBaseStructure.TIM_Prescaler = 0;
TIM_TimeBaseStructure.TIM_Period = Period - 1;
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM10, &TIM_TimeBaseStructure);
/* Enable TIM10 Preload register on ARR */
TIM_ARRPreloadConfig(TIM10, ENABLE);
/* TIM PWM1 Mode configuration */
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = Period / 2; // 50%
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
/* Output Compare PWM1 Mode configuration: Channel1 PB.8 */
TIM_OC1Init(TIM10, &TIM_OCInitStructure);
TIM_OC1PreloadConfig(TIM10, TIM_OCPreload_Enable);
/* TIM10 enable counter */
TIM_Cmd(TIM10, ENABLE);
}
/**************************************************************************************/
int main(void)
{
RCC_Configuration();
GPIO_Configuration();
TIM10_Configuration();
while(1); // Don't want to exit
}
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..