cancel
Showing results for 
Search instead for 
Did you mean: 

PWM channels of STM32G474. Is this the right MCU ?

JJ..1
Associate II

Greetings,

I need to provide PWM signals for 36 and 34 Outputs. Both the cases have been described under. Kindly note that all the outputs are independently operated.

I need to know if STM32G474 can address to the job?

CASE 1:

These are the list of 6 PWN signals of 12 V that are in use.

1) 100% i.e 12V equivalent

2) 75% i.e 9V equivalent

3) 50% i.e 6V equivalent

4) 41.66% i.e 5V equivalent

5) 33.3% i.e 4V equivalent

6) 25V% i.e 3V equivalent

There are 36 Outputs.

1) 1 output (fan motor) would only receive 3V to 5V equivalent PWN signa, which ever is called for

2) 1 Output (fan motor) would only receive 6V to 12V equivalent PWN signal, which ever is called for

3) 34 Outputs (solenoid valves) receive 100% or 33.3% PWM independently. First 100% for 100ms to turn on then 33.3% to remain ON.

CASE 2:

I can even work with 2 PWM signals

1) 100%

2) 33.3%

This will be used for 34 outputs (solenoid Valves). Outputs receive 100% or 33.3% PWM independently. First 100% for 100ms to turn on then 33.3% to remain ON.

Are any of the cases possible using the mentioned MCU?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
berendi
Principal

As I've written in my previous answer, any STM32 MCU can do it with 3 DMA channels outputting to GPIO (or 2 DMA channels and a single 4 channel timer).

https://community.st.com/s/question/0D50X0000C4Nw8DSQS/salutationsi-need-guidance-to-choose-a-micro-controller-that-can-communicate-with-stm32f103vct6-at-the-same-speed-through-uart-and-has-36-pwn-pinsthank-youj