2016-02-21 3:13 PM
Hello,
I need to generate sin wave using STM32 uC. Now here comes the problem. I am able to obtain the required sin wave with the required frequency and the required amplitude however there are other (more than one) frequency components.After spending some time, I think I have pinpointed my problem down to having something related to 'jitter' in the PWM or phase noise because of a mismatched PWM frequency and sample rate of the lookup table.What do you think? Any help would be appreciated!2016-02-24 10:23 PM
I tried the code but I didn't see any output from both pins (1 & 1N). I think it is still in high impedance mode. Can you send me the source code please and tell me what you tried to change?
2016-02-25 1:25 PM
@clive1, any clue of how i should proceed?
Your help is much appreciated. Thank you.