2016-02-21 3:13 PM
Hello,
I need to generate sin wave using STM32 uC. Now here comes the problem. I am able to obtain the required sin wave with the required frequency and the required amplitude however there are other (more than one) frequency components.After spending some time, I think I have pinpointed my problem down to having something related to 'jitter' in the PWM or phase noise because of a mismatched PWM frequency and sample rate of the lookup table.What do you think? Any help would be appreciated!2016-02-21 4:47 PM
Ultimately the machine does what you tell it too, unfortunately I can't see from this what you're physically instructing the machine to do.
Instead of programming the timer, write all the data you generate to a file, and the plot and review that.2016-02-23 1:55 PM
I have a sinusoidal lookup table that contains only a 50Hz that I'm using, however I don't know how its not only 50Hz on the capacitor of the lowpass filter. If you need details of the setup see my previous post.
Thanks!2016-02-23 5:17 PM
Ok, the key detail missing is the code, something I can compile and follow the logic, I'm not looking to recreate or resolve this for myself.
2016-02-24 12:22 PM
2016-02-24 12:47 PM
Your update interrupt looks really dodgy
//update sin sample on overflow only if(htim8.Instance->CNT > 3000){ //... And 4200 is half of 8400 Needs to beif (__HAL_TIM_GET_IT_SOURCE(&htim8, TIM_IT_UPDATE))
{
__HAL_TIM_CLEAR_IT(&htim8, TIM_IT_UPDATE);
if (sin_index >= 200)
sin_index = 0;
__HAL_TIM_SetCompare(&htim8, TIM_CHANNEL_1, 4200 + sin_wave_50hz[sin_index++]); //4200 = PERIOD/2 = 8400/2
}
2016-02-24 1:14 PM
2016-02-24 3:45 PM
I'm not sure how it is going to underflow, the update occurs once per period, ie at 10 KHz
Realistically this could be done with DMA and be completely autonomous.2016-02-24 5:15 PM
Other thoughts, the Period should be N-1, the TIM8 will run at 168 MHz
Attached is a .HEX that drives PC6 (TIM8_CH1) and PA7 (TIM8_CH1N), this should generate a 50 Hz sine wave via a 10 KHz PWM. Please see if this generate the wave form you expect. ________________ Attachments : PWM8_50HZ_REL1.hex : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I12Q&d=%2Fa%2F0X0000000bhN%2FAlv3B8cCDLf9hMbKFwEV.s6SQFd0RrtTqBJiz4KPsl8&asPdf=false2016-02-24 10:13 PM
Underflow can occur because I have my timer running in up-down mode counter.