PWM 3 channel with shift phase 120 degree
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-05-02 7:41 AM
Posted on May 02, 2015 at 16:41
Hi.
I am working with STM32F4 MCU and looking for help in the next question: I need to do PWM 3 channel with shift phase 120 degree on the start PWM operation. For example, PWM CH1 with 0 degrees, PWM CH2 with 120 degrees and PWM CH2 with 240 degrees.Every PWM GPIOs are configured to start from 'Low' to 'High'. (This is OK). The problem is: When I configure 120 degrees shit for 40 KHz it calculated as 120 degrees shift from half time (the time that PWM is in the 'High' state). This means that shit between PWM channels is 60 degrees (4.2us) instead 120 degrees (8.4us). When I tried to multiply period as: TIM_OCInitStructure.TIM_Pulse = ((Period*2 * 3) / 3) - 1 this is does not work.Where is my problem?My email is tropinka06@gmail.com.I know that there are similar posts, but no one with the same problem.Thank you.Evgeni KosakovskiFor this I use the next code:void GPIO_Configuration(void){ GPIO_InitTypeDef GPIO_InitStructure; /* GPIOE Configuration: TIM1 on PE9/PE10/PE13 */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_11 | GPIO_Pin_13; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN; GPIO_Init(GPIOE, &GPIO_InitStructure); /* Connect TIM1 pin */ GPIO_PinAFConfig(GPIOE, GPIO_PinSource9, GPIO_AF_TIM1); // PE9 TIM1_CH1 GPIO_PinAFConfig(GPIOE, GPIO_PinSource11, GPIO_AF_TIM1); // PE11 TIM1_CH2 GPIO_PinAFConfig(GPIOE, GPIO_PinSource13, GPIO_AF_TIM1); // PE13 TIM1_CH3 } //****************************************************************************** void TIM1_Configuration(uint32_t PWM_Frequency){ RCC_ClocksTypeDef RCC_ClocksStructure; TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_OCInitTypeDef TIM_OCInitStructure; int Prescaler, Period; uint32_t TimerFrequency = 0; // Get clocks RCC_GetClocksFreq(&RCC_ClocksStructure); // For TIM1 TimerFrequency = RCC_ClocksStructure.HCLK_Frequency; Prescaler = 1; Period = TimerFrequency / 2 / PWM_Frequency; // KHz // The toggle halves the frequency /* Time base configuration */ TIM_TimeBaseStructure.TIM_Period = Period - 1; TIM_TimeBaseStructure.TIM_Prescaler = Prescaler - 1; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure); /* Output Compare Toggle Mode configuration: Channel 1, 2 and 3 */ TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Toggle; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_OutputNState = TIM_OutputNState_Enable; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OCInitStructure.TIM_OCNPolarity = TIM_OCPolarity_High; /* Default unused fields TIM1 more sensitive */ TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Set; TIM_OCInitStructure.TIM_OCNIdleState = TIM_OCNIdleState_Reset; /* Don't want to set 0 or Period, but have 3 points at 120 degrees from each other */ TIM_OCInitStructure.TIM_Pulse = ((Period * 1) / 3) - 1; TIM_OC1Init(TIM1, &TIM_OCInitStructure); TIM_OCInitStructure.TIM_Pulse = ((Period * 2) / 3) - 1; TIM_OC2Init(TIM1, &TIM_OCInitStructure); TIM_OCInitStructure.TIM_Pulse = ((Period * 3) / 3) - 1; TIM_OC3Init(TIM1, &TIM_OCInitStructure); /* Enable pins, TIM1 more sensitive */ TIM_CtrlPWMOutputs(TIM1, ENABLE); /* TIM1 enable counter */ TIM_Cmd(TIM1, ENABLE);}int main(void){ SysTickConfig(); RCC_Configuration(); GPIO_Configuration(); TIM1_Configuration(40000); // 40KHz while (1) {}}
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-05-21 5:25 AM
Posted on May 21, 2015 at 14:25I think you find wrong periodPeriod = (timerfrequency / 2) / pwm_frequencyjust a suggestion