Skip to main content
mete
Senior
November 20, 2023
Solved

purpose of RCC_RSR_RMVF

  • November 20, 2023
  • 5 replies
  • 2648 views

I read RCC RSR to determine the cause of reset. It is not clear to me the purpose of RMVF bit. I guess it resets the other flags but why would I want that ? I wonder if I am missing something.

This topic has been closed for replies.
Best answer by STTwo-32

After a reset happens, the reset flag will be set and will keep set until we clear it using the RMVF bit. If we don't, we will not be able to detect the next reset coming from the same source (because the flag will keep set and we will never now if it is the first reset or  an other one). 

Best Regards.

STTwo-32

5 replies

STTwo-32
ST Technical Moderator
November 20, 2023

Hello @mete 

Thank you for reporting this. I will check it internally and get back to you as soon as possible.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
STTwo-32
ST Technical Moderator
November 20, 2023

Hi @mete  

The RMVF bit of the RCC_RSR is Set and reset by software to reset the value of the reset flags since those flags are read only so we need to reset them using an external source (wish is the RMVF in this case). 

For the Typo in the RM0481 Rev 1 (the RCC reset status register (RCC_RSR) bits [26,31] should be read only (r) not read/write (rw). I've escalated this to the appropriate team for correction of UM3115 with internal ticket ID166678.

(PS: ID166678 is an internal tracking number and is not accessible or usable by customers)

thank you for your contribution.

Best Regards.

STTwo-32.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
mete
meteAuthor
Senior
November 20, 2023

Thanks @STTwo-32 , what I do not understand is why I would want to reset the status of reset flags. Do they not always reflect the reset status after a reset happens ? For what reason would I need to reset it manually using RMVF ?

STTwo-32
STTwo-32Best answer
ST Technical Moderator
November 20, 2023

After a reset happens, the reset flag will be set and will keep set until we clear it using the RMVF bit. If we don't, we will not be able to detect the next reset coming from the same source (because the flag will keep set and we will never now if it is the first reset or  an other one). 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.