2013-08-07 01:35 AM
Hello,
I equipped the Header of the STM32F100RB-VL Dicovery Board with some LEDs. But then I recognised that PB3 and PB4 are not working, because they have to be remapped. Since this remapping I`m not able to flash the Discovery Board again. I read the notice in application note ''Once the JTAG I/Os are disabled, connection with the host debugger is lost and cannot be re-established as long as the JTAG I/Os remain disabled''
I don`t know how to fix this. I`m working with Keil µVision. Any Ideas? Thank`s in advance.2013-08-07 03:28 AM
solved