cancel
Showing results for 
Search instead for 
Did you mean: 

Program Upload method in nucleo stm32f103

yugi
Associate

Hello Everyone 
I am try to upload my code through stm32f103 necleo debuger or programmer but  have facing one issue for no st link found error 
I have attached the pic please give the solution .

4 REPLIES 4
AScha.3
Chief II

Hi,

Was the nucleo/st-link working before ?

With same USB cable ?

If remove your external wires, then working?

If you feel a post has answered your question, please click "Accept as Solution".
Andrew Neil
Evangelist III

@yugi wrote:

 no st link found error 
I have attached the pic please give the solution .


Is the ST-Link being detected by the host computer?

eg, does the Virtual COM Port appear in the Device Manager?

AndrewNeil_0-1706630498139.png

If the host computer isn't detecting the ST-Link, then there's no way that any other app (eg, debugger or programmer) is going to be able to use it.

#STLinkVCP #STLinkComPort #DeviceManager

i'm check the stlink  in device manager is showing the stlink

 

Show a screenshot of the message(s) you receive

BTW: you can just paste an image into the post (as I did above) - no need to attach.