cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with working on 2.5V

Artem Dmitriev
Associate II
Posted on March 01, 2018 at 11:10

Hello!

On the PCB from LDO(

MCP1700T-3302E

) 3.3V are supplied 2 chips:

GPS

:

SIM

68

M,

STM32L475RET6.

GPS power supply is controlled by STM.

When STM turn on GPS module voltage temporarily drops to 2,5V.

At this time MCU works incorrectly if frequency is 80MHz (hang or HardFault handler are called). If frequency 40Mhz all fine.

What could be the problem?

0690X00000604QlQAI.jpg

0690X00000604QqQAI.jpg

Note: this post was migrated and contained many threaded conversations, some content may be missing.
30 REPLIES 30
Dvorak.Peter
Senior II
Posted on March 06, 2018 at 13:36

Replacing your GPS power switch with the following device will reduce your power supply disturbance and solve all your problems

The TI TPS2051B power-distribution switches are 

intended for applications where heavy capacitive

loads and short circuits are likely to be encountered.

These devices incorporates 70-mΩ N-channel

MOSFET power switches for power-distribution

systems that require multiple power switches in a

single package. Each switch is controlled by a logic

enable input. Gate drive is provided by an internal

charge pump designed to control the power-switch

rise times and fall times to minimize current surges

during switching. The charge pump requires no

external components and allows operation from

supplies as low as 2.7 V.