2014-06-30 1:08 PM
Hi.
I use a STM32F103ZE microcontroller.I try to change the System Clock (default is HSI) to HSE.On my board is a HSE - cristal oscilator which value is 8 Mhz and i want to change it to 72 Mhz and it works.But if i want to change it to a small value , for instance 24 Mhz i cannot change it, even if i made the setup (RCC->CFGR |= (1 << 16) | (1 << 18); ).One more quetion : how many clock cycles takes to execute an instruction ?#include<stm32f10x.h>void wait(void) { int d; for(d = 0; d < 1000000; d++); }int main (void) { unsigned int i; RCC->CR &= ~(1 << 0); RCC->CR |= (1 << 19); RCC->CR &= ~(1 << 16); RCC->CR &= ~(1 << 24); RCC->CFGR &= ~(1 << 17); RCC->CFGR |= (1 << 0); RCC->CFGR &= ~(1 << 1); RCC->CFGR |= (1 << 16) | (1 << 18) | (1 << 19) | (1 << 20); RCC->CFGR |= (1 << 25) | (1 << 26); RCC->CR |= (1 << 24); RCC->CR |= (1 << 16); RCC->APB2ENR |= (1UL << 7); // Enable GPIOF GPIOF->CRL = 0x33000000; // PF.6, PF.7 defined as Outputs GPIOF->CRH = 0x33; // PF.8, PF.9 defined as Outputs while (1) { for(i = 1<<6; i < 1<<10; i <<= 1) { GPIOF->BSRR = i; // Turn LED on wait(); GPIOF->BRR = i; // Turn LED of } }}2014-06-30 2:45 PM
One more question : how many clock cycles takes to execute an instruction ?
It's pipelined, so each instruction takes several cycles, though the throughput is usually one cycle. Loads from slow buses and memories will delay things, divides can take between 2 and 12 cycles. This is for machine instructions, not C code lines