Problem with multiple EXTI on the same Port
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-08-19 2:34 PM
Posted on August 19, 2013 at 23:34
Hey guys !
I have a problem with my STM32F100 Board - I'd like to have PC.0 as EXTI_Line_0 and PC.1 as EXTI_Line_1. Here is my configuration:
EXTI_InitTypeDef EXTI_InitStructure;
NVIC_InitTypeDef NVIC_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
/* Enable GPIO Port C */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC,ENABLE);
/* PC.12 as Output (LED) */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;
GPIO_Init(GPIOC, &GPIO_InitStructure);
/* Inputs and EXTI */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 ;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;
GPIO_Init(GPIOC, &GPIO_InitStructure);
/* Selects PC Pins as EXTI Lines */
GPIO_EXTILineConfig(GPIO_PortSourceGPIOC, GPIO_PinSource0);
GPIO_EXTILineConfig(GPIO_PortSourceGPIOC, GPIO_PinSource1);
/* Configure two bit for preemption priority */
NVIC_PriorityGroupConfig(NVIC_PriorityGroup_2);
/* EXTI */
NVIC_InitStructure.NVIC_IRQChannel = EXTI0_IRQChannel;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
NVIC_InitStructure.NVIC_IRQChannel = EXTI1_IRQChannel;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
EXTI_InitStructure.EXTI_Line = EXTI_Line0; // PC.0
EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt;
EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising;
EXTI_InitStructure.EXTI_LineCmd = ENABLE;
EXTI_Init(&EXTI_InitStructure);
EXTI_InitStructure.EXTI_Line = EXTI_Line1; // PC.1
EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt;
EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising;
EXTI_InitStructure.EXTI_LineCmd = ENABLE;
EXTI_Init(&EXTI_InitStructure);
The IRQ Handlers are configured to do nothing but toggle a LED:
void EXTI0_IRQHandler(void)
{
if(EXTI_GetITStatus(EXTI_Line0) != RESET)
// Ensure get EXTI line 0 pending bit
{
GPIO_WriteBit(GPIOC,GPIO_Pin_12, 1);
EXTI_ClearITPendingBit(EXTI_Line0);
// Clear the EXTI line 0 pending bit
}
}
void EXTI1_IRQHandler(void)
{
if(EXTI_GetITStatus(EXTI_Line1) != RESET)
// Ensure get EXTI line 1 pending bit
{
GPIO_WriteBit(GPIOC,GPIO_Pin_12, 0);
EXTI_ClearITPendingBit(EXTI_Line1);
// Clear the EXTI line 1 pending bit
}
}
My problem now is, that EXTI1 IRQ handler is never executed, and EXTI0 IRQ is executed by PC.1!
How is this possible? Did I forget something in the configuration?
I am assuming that the wiring is correct.
thanks in advance
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-08-19 4:28 PM
Posted on August 20, 2013 at 01:28
/* Enable AFIO clock */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO, ENABLE); Otherwise doesn't look unreasonable You do look to be using an older firmware library. NVIC_InitStructure.NVIC_IRQChannel = EXTI0_IRQn; NVIC_InitStructure.NVIC_IRQChannel = EXTI1_IRQn; What are the pin states actually doing? Do you need pull up/down settings, or have them externally, diagram circuit.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-08-20 10:45 AM
Posted on August 20, 2013 at 19:45
Two Sensors (24VDC) with each a resistor and a Z-DiodeEDIT:The Programm is also going through the if(EXTI_GetITStatus(EXTI_Line0) != RESET) part - also in the wrong IRQ Handler - wich confuses me?!?
Now I have the same code just with AFIO Clock enabled.
Both Interrupts are now working, but each Interrupt opens both IRQ Handlers. It's own first, and then the other one. Do I have something wrong with my board? Resistance between PC.0 and PC.1 is >0,7MOhm - so this should be OK. When I put a Voltage of 3V3 on PC.0 - PC.1 is under 0,05V and vice versa.Design is as followed:Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-10-28 12:15 PM
Posted on October 28, 2014 at 20:15
Hi,
Were you able to find out why pressing one key generates an interrupt on the correct pin but also on the other pin? I am facing something similar using PB12-15 on EXTI15_10_IRQHandler Pressing PB12 for example generated an interrupt on this one as well as the others.Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-10-28 12:57 PM
Posted on October 28, 2014 at 20:57
Are you seeing this on an STM32F1 also?
I haven't tried this but looks like it should be easy enough to replicate/validate
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-10-28 8:04 PM
Posted on October 29, 2014 at 04:04
Hi,
I am seeing this problem on the STM32VL discovery board. Once in the EXTI ISR, I disable the interrupt and clear the pending bit. Is this the right way to disable the interrupt?void EXTI15_10_IRQHandler(void)
{
DisableButton_IRQ(EXTI15_10_IRQn); // Disable interrupt to avoid any debounce effects
if(EXTI_GetITStatus(EXTI_Line12) != RESET) {
EXTI_ClearITPendingBit(EXTI_Line12); // Clear the EXTI line 12 pending bit
keyIndex=0;
keyPin = KEYPAD_COL1;
} else
=====================
void DisableButton_IRQ(uint8_t interupt_num){
NVIC_InitTypeDef NVIC_InitStructure;
/* Disable and set EXTI10_15 Interrupt to the lowest priority */
NVIC_InitStructure.NVIC_IRQChannel = interupt_num;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x0F;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x0F;
NVIC_InitStructure.NVIC_IRQChannelCmd = DISABLE;
NVIC_Init(&NVIC_InitStructure);
}