cancel
Showing results for 
Search instead for 
Did you mean: 

P-NUCLEO-LRWAN2 Board Stuck at "Ethernet Starting"

Hari-Senstornet
Visitor

Hello,

I am using the P-NUCLEO-LRWAN2 board for LoRaWAN development. While booting up the device, it always gets stuck at the message

Powered by RisingHF & STMicroelectronics
-------------------------------------------------------------------------------
VERSION: 2.1.7, Nov 6 2018
LOG: OFF
AT ECHO: ON
BAUDRATE: 115200bps
MACADDR: 08:00:27:0C:23:38
ETHERNET: DHCP
DNS1: 114.114.114.114
DNS2: 8.8.8.8
NTP SERVER: 1.ubuntu.pool.ntp.org
EUI PADDING: {3, FF}, {4, FF}
GATEWAY ID: 080027FFFF0C2338
LORAWAN: Public
LORAWAN SERVER: router.eu.thethings.network
UPLINK UDP PORT: 1700
DOWNLINK UDP PORT: 1700
CHANNEL0: 867100000, A, SF7/SF12, BW125KHz (LORA_MULTI_SF)
CHANNEL1: 867300000, A, SF7/SF12, BW125KHz (LORA_MULTI_SF)
CHANNEL2: 867500000, A, SF7/SF12, BW125KHz (LORA_MULTI_SF)
CHANNEL3: 867700000, A, SF7/SF12, BW125KHz (LORA_MULTI_SF)
CHANNEL4: 867900000, A, SF7/SF12, BW125KHz (LORA_MULTI_SF)
CHANNEL5: 868100000, B, SF7/SF12, BW125KHz (LORA_MULTI_SF)
CHANNEL6: 868300000, B, SF7/SF12, BW125KHz (LORA_MULTI_SF)
CHANNEL7: 868500000, B, SF7/SF12, BW125KHz (LORA_MULTI_SF)
CHANNEL8: 868300000, B, SF7, BW250KHz (LORA_STANDARD)
CHANNEL9: 868800000, B, 50Kbps (FSK)
-------------------------------------------------------------------------------
Concentrator starting...
Concentrator Radio A type SX1257
Concentrator Radio B type SX1257
Concentrator started (2926ms)
ST LoRa GW V2
Ethernet starting...

After this point, the board does not proceed further.

Troubleshooting Done:

  • Tried rebooting multiple times.

  • Verified network cable and DHCP server are working fine.

  • Tried connecting to different routers/networks.

  • Reflashes firmware with the same version.
    Board Details:

    • P-NUCLEO-LRWAN2

      I am not sure if this is an issue with firmware, hardware, or network configuration. Could you please help me troubleshoot or suggest further debugging steps?

      Thank you.

      Regards,
      Hari Prasath P
      Firmware Engineer
      Senstornet Technologies
      Chennai - India




0 REPLIES 0