2016-02-07 12:54 AM
Hi
I configured 2 EXTI (PA0 & PB1 ) and work perfectly. But when I configure Port B pins output and connect a led to them ( or even a wire!) inerrupts occure! (I pulled up intrnally and externally PA0 & PB1 and in port B I used SPI) can any one help me to use other pins of port B?2016-02-08 01:43 AM
Bit confusing.Try to see on CRO if some noise is coming on GPIO, or send your piece of code.
/*Please
mark helpfull
if this post helps you or solves your problem.*/
/**disclaimer**/
/* I am not a person from ST Technical Support Team. So please verify/test any support/suggestion at your end.*/
/* This post is only for general support purpose and free of any charge.If you need any personal support for your work please contact at
embeddeddesign.help@gmail.com
*/