Skip to main content
BBori.1
Associate II
November 27, 2020
Solved

Problem with include

  • November 27, 2020
  • 2 replies
  • 1300 views

Hello, I'm having troubles with a library in C

I've made a library named "LedControl" divided in "LedControl.h" and "LedControl.c"

So far the header file is like this:

#ifndef SRC_CUST_LEDCONTROL_H_
#define SRC_CUST_LEDCONTROL_H_
 
 
 
 
#define LC_POINTER_LIST_LEN 255
 
 
 
//					 VAL1 VAL2 END ON/OFF TR1 TR0 PWMv FLOAT 32 CHANGE
uint8_t WORD_IT[] = {0x00, 0x01, 0xFF, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
uint8_t WORD_IS[] = {0x03, 0x04, 0xFF, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
uint8_t WORD_TWENTY_MINUTES[] = {0x0D, 0x0E, 0x0F, 0x10, 0x11, 0x12, 0xFF, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
uint8_t WORD_TWENTYFIVE_MINUTES[] = {0x0D, 0x0E, 0x0F, 0x10, 0x11, 0x12, 0x13, 0x14, 0x15, 0x16, 0x17, 0xFF, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
uint8_t WORD_FIVE_MINUTES[] = {0x14, 0x15, 0x16, 0x17, 0xFF, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
 
//[... more array definitions]
 
void LC_transitionIn(uint8_t *chars, uint16_t time);
 
void LC_transitionOut(uint8_t *chars, uint16_t time);
 
void LC_Control_tick();
 
 
 
 
 
 
#endif /* SRC_CUST_LEDCONTROL_H_ */

And the source file is just:

#include "LedControl.h"
 
 
void LC_Control_tick()
{
 
}

Problem is, when I try yo compile I get an error for each variable declaration in the header file like this:

../Core/Src/cust/LedControl.h:129:22: error: unknown type name 'uint8_t'

I figured "ok, I just add #incldue <stdint.h> in my source file like this:

#include <stdint.h>
#include "LedControl.h"
 
 
void LC_Control_tick()
{
 
}

And then I get a whole bunch of error like this (one per variable declaration)

Core/Src/main.o:C:/CubeProj/RelojN/Debug/../Core/Src/cust/LedControl.h:125: multiple definition of `WORD_WKD_SU'

Core/Src/cust/LedControl.o:C:/CubeProj/RelojN/Debug/../Core/Src/cust/LedControl.h:125: first defined here

The header file LedControl.h is only being included once in my main file, and it has a #Ifdef​ right in the header!

I have to add that I allready have other source and header files in the same project included in the exact same way that also use uint8_t and they work just fine

Thank you!

    This topic has been closed for replies.
    Best answer by KnarfB

    You should read a basic book on C first. Variable definition in header files is nonsense.

    2 replies

    KnarfB
    KnarfBBest answer
    Super User
    November 27, 2020

    You should read a basic book on C first. Variable definition in header files is nonsense.

    BBori.1
    BBori.1Author
    Associate II
    November 27, 2020

    Got it! thanks!