2010-03-24 12:39 PM
Problem with assert_param
2011-05-17 04:44 AM
Change the #ifdef USE_FULL_ASSERT to #ifdef DEBUG, like in good old library 2.0, or simply #define USE_FULL_ASSERT yourself or put USE_FULL_ASSERT in the C/C++ preprocessor macro definitions.
2011-05-17 04:44 AM
That was what I did but the error still persist...
I don't know what more can I do...
I tried defining
DEBUG
instead ofUSE_FULL_ASSERT
as you suggested and I also tried to define it in C/C++ compiler macros but no way...Why you said ''like in good old library 2.0''? 3.2.0 is not a good one?
Thanks for replying edison!
Anyone can suggest something? I'm really lost...
2011-05-17 04:44 AM
This is where it pays to understand how the whole preprocessor-compiler-linker process works.
If the Linker is giving you this error, it means that the Compiler has generated calls to assert_param as if it were a function. This means that your macro definition is not working properly! To sort out preprocessor problems like this, find out (in the Compiler Manual) how to view the preprocessor output...2011-05-17 04:44 AM
Hi again,
Ok, I did what Neil said and now I can view the preprocessor files (.i). What should I check? How can I know if a macro is working properly?
Thanks!!
2011-05-17 04:44 AM
''How can I know if a macro is working properly?''
You do understand what macros are supposed to do, don't you? So, if they do that, then we say that they are ''working'' !!😉
To recap, a macro is a text substitution - so, instead of seeing ''assert_param'' in the pre-processed text, you should see its expansion. If you are still seeing ''assert_param'' in the pre-processed text, then the preprocessor has not expanded it; ie, it has not worked as a macro!
2011-05-17 04:44 AM
Ooooook!!!
Thanks, Neil. I think I am still a noob on C programming. Ok, now I know what the problem exactly is. I can see
assert_param
in the preprocessor files so that means whant Neil said, the macro ''is not working''. Now the problem is how to fix it.I'm going to find whether it is possible to disable/enable macros in EWARM. Maybe is a configuration parameter I forgot... Any other idea?
Thanks again Neil!
2011-05-17 04:44 AM
''I think I am still a noob on C programming''
Note that this is standard 'C' stuff - nothing specifically to do with STM32, IAR, or embedded. Therefore any 'C' textbook should help... ''I'm going to find whether it is possible to disable/enable macros in EWARM.'' No, that is not the correct approach! What you need to do is to find out how to correctly configure your Project so that the macro works! Note that the macro definition is contained within #ifdef USE_FULL_ASSERT This means that the definition is effective only if the symbol USE_FULL_ASSERT is defined...
2011-05-17 04:44 AM
Note that there is also a #else which should create a ''null'' definition when USE_FULL_ASSERT is not defined.
The fact that you're getting neither the ''full'' definition nor the ''null'' definition - so that the compiler thinks it's a function call - suggests that you are not actually including this at all...2011-05-17 04:44 AM
What I did now is that:
/* Exported macro ------------------------------------------------------------*/
#ifdef USE_FULL_ASSERT
#define assert_param(expr) ((expr) ? (void)0 : assert_failed((uint8_t *)__FILE__, __LINE__))
#error ----------------------------------------------------- assert full def.
/* Exported functions ------------------------------------------------------- */
void assert_failed(uint8_t* file, uint32_t line);
#else
#define assert_param(expr) ((void)0)
#error ----------------------------------------------------- assert null def.
#endif /* USE_FULL_ASSERT */
The compiler return first error, so that means that I am including it (maybe I'm wrong?)
Thaaaaaanks!!