2013-03-20 11:17 AM
hi
now I
am trying to
achieve
a
basic
equipment
card
STM31
-P103Olimex
of
(
STM32F103RB
microcontroller
),I used
the
Flash
loader
demonstrator
program
for
the card (
boot0=1boot1
= 0) and i chose COM3, baude=115200, parity=None, Echo=Disable, Time out=10
but it always
displays the
following error
:''no response from the target the boot loader can not be startedthank you for
your help''
thank you for
your help.
2013-05-03 03:20 AM
thank you clive for your help.
I have a problem
with
SD
card,
at first
I used
the
mikroC
PRO
FOR ARM
,the SD card
it works
fine, but the
problem
is
that
software is limited
(
licenserequired
)and for this
I used
Coocox
COIDE
as
software
but I can not
to solve
the problem
of the SD Card
, Ialready
apply
to
problem
in the
forum
COOCOX
but people
noreplied
.I need
an example of
SD
CARD and
thank you
for your help
??2013-05-03 06:46 AM
I need
an example of
SD
CARD and
thank you
for your help
?? I'm not currently doing engineering or porting work on the F1 platform. STM32F10x_StdPeriph_Lib_V3.5.0\Project\STM32F10x_StdPeriph_Examples\SDIO\uSDCard\main.c2013-05-20 01:59 AM
I have another
question.
I need
to put my
card
STM32
-
P103standby
I
test the
consumption of all
the
card
I see that
it
uses up to
19mA
but
the literature indicates that
standby power
consumption must
be
to
some
uA
.here is my code
:
#include ''stm32f10x.h'' #include ''stm32f10x_gpio.h'' #include ''stm32f10x_rcc.h'' #define LED_PORT GPIOC GPIO_InitTypeDef GPIO_InitStructure; ErrorStatus HSEStartUpStatus; void RCC_Configuration(void); void GPIO_Configuration(void); void main(void) { RCC_Configuration(); GPIO_Configuration(); PWR_EnterSTANDBYMode(); while (1) { } } void RCC_Configuration(void) { RCC_DeInit(); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB | RCC_APB2Periph_GPIOC | RCC_APB2Periph_GPIOD | RCC_APB2Periph_GPIOE | RCC_APB2Periph_AFIO, ENABLE); } void GPIO_Configuration(void) { GPIO_InitStructure.GPIO_Pin = GPIO_Pin_All; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_Init(GPIOB, &GPIO_InitStructure); GPIO_Init(GPIOC, &GPIO_InitStructure); GPIO_Init(GPIOD, &GPIO_InitStructure); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB | RCC_APB2Periph_GPIOD | RCC_APB2Periph_GPIOE, DISABLE); ADC_Cmd(ADC1, DISABLE); } and thank you for your help