problem in using (hal_stm32f4xx library) to read value written to user configured sector of flash
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-03-22 9:57 AM
can any one help me with this problem? I try to make sure that I stored a value correctly in the user _configured section of flash .So I read value from a specific address of flash memory immediately after programming it through hal_stm32f4xx library. For debugging I make condition on the read value if it equals the value written to the address a led turns on. I have no problem while debugging and running without optimizations. But when I chose to run (the most optimized version of the code
without any debugging)
from the project settings , the led didn't turn on. and this is the source code __attribute__((__section__(''.user_data''))) const uint32_t userConfig[64]; uint32_t testreadvalue=0; uint32_t testwritevalue=6; HAL_StatusTypeDef status = HAL_ERROR;void testreadFlash(void)
{ testreadvalue =*(uint8_t *)userConfig; } void testwriteFlash(void) { HAL_StatusTypeDef status; status = HAL_FLASH_Unlock(); // returnsHAL
_OK FLASH_Erase_Sector(FLASH_SECTOR_2, VOLTAGE_RANGE_1); status = HAL_FLASH_Program(TYPEPROGRAM_HALFWORD, (uint32_t) userConfig, (uint64_t)testwritevalue);// returns
HAL
_OK status = HAL_FLASH_Lock();// returns
HAL
_OK } int main(void) { HAL_Init();SystemClock_Config();
MX_GPIO_Init();testwriteFlash();
testreadFlash(); if(testreadvalue==6) { HAL_GPIO_WritePin(GPIOB,GPIO_PIN_10,0);}// turn on the yellow led
else{ HAL_GPIO_WritePin(GPIOB,GPIO_PIN_10,1);}
// turn off the yellow led
while (1) {} } Thanks in advance- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-03-22 10:12 AM
[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/problem%20with%20restoring%20value%20written%20to%20user%20configured%20flash%20after%20power%20reset&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx?Paged%3DTRUE%26p_StickyPost%3D%26p_DiscussionLastUpdated%3D20150319%252018%253a05%253a33%26p_ID%3D51603%26View%3D%257bF47A9ED8%252dE726%252d42BE%252dACED%252d732F13B66581%257d%26FolderCTID%3D0x012001%26PageFirstRow%3D41¤tviews=9]Earlier duplicate thread
Not sure there's much HAL support here in the pro user space. Might I suggest you check the value first and not write it every pass, review the error status at each step, printing the result to a serial console, and not trying to write if the memory isn't the 0xFF state, or the erase fails..Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-03-22 10:57 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-03-23 3:04 AM
I detected that the sector isn't erased successfully while running the optimized version of the code by running a buzzer if the memory isn't 0xFF
what to do if the erase fails. But while running the non optimized version of the code the sector is erased succssessfully.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-03-23 4:23 AM
What toolchain are you using? Are you sure you can't provide some serial connectivity so you can get more informative feedback than a buzzer?
I think you need to make sure you clear any error/status states from the flash controller after you unlock it for the first time. In SPL terms this would look likeFLASH_Unlock();
FLASH_ClearFlag(FLASH_FLAG_BSY | FLASH_FLAG_EOP | FLASH_FLAG_PGERR | FLASH_FLAG_WRPRTERR);
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-03-23 4:38 AM
I'm using the toolchain ARM_GNU_GCC.
In the start and after each operation,I clear the flags, execute
and checkfor errors.
This is the up_to_date version of the test_write_flash() function void testwriteFlash(void) { status1 = HAL_FLASH_Unlock(); FLASH->CR |= 0x3000000; // Enable End of operation and errors interrupts FLASH_ClearFlag(FLASH_FLAG_BSY | FLASH_FLAG_EOP | FLASH_FLAG_PGERR | FLASH_FLAG_WRPRTERR); FLASH_Erase_Sector(FLASH_SECTOR_2, VOLTAGE_RANGE_1); if(__HAL_FLASH_GET_FLAG((FLASH_FLAG_OPERR | FLASH_FLAG_WRPERR | FLASH_FLAG_PGAERR | \ FLASH_FLAG_PGPERR | FLASH_FLAG_PGSERR | FLASH_FLAG_RDERR)) != RESET) { Run_Buzzer();// No sound emitted here if put alone without next conditions } if(testreadvalue!=255)
{ Run_Buzzer(); // sound emitted here if put alone without other conditions } else { __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_OPERR | FLASH_FLAG_WRPERR | FLASH_FLAG_PGAERR |FLASH_FLAG_PGSERR ); status2 = HAL_FLASH_Program(TYPEPROGRAM_HALFWORD, (uint32_t) userConfig, (uint64_t)testwritevalue); if(__HAL_FLASH_GET_FLAG((FLASH_FLAG_OPERR | FLASH_FLAG_WRPERR | FLASH_FLAG_PGAERR | \ FLASH_FLAG_PGPERR | FLASH_FLAG_PGSERR | FLASH_FLAG_RDERR)) != RESET) { Run_Buzzer();// No sound emitted here if put alone without the previous conditions } __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_OPERR | FLASH_FLAG_WRPERR | FLASH_FLAG_PGAERR |FLASH_FLAG_PGSERR ); } status3 = HAL_FLASH_Lock(); } }