Problem! flash loader doesn't work after I jump to bootloader in stm32f446rc
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-10 10:06 AM
Hello, I have a board with stm32f446rc processor and I don't get to connect bootloader with stm32 flashloader.
Following below this function used to access the bootloader on chip. I am using USART1 (PA9,PA10) to connect RS232.
void JumpToBootloader(void) {
void (*SysMemBootJump)(void);/**
* Step: Set system memory address. * * For STM32F446, system memory is on 0x1FFF 0000 * For other families, check AN2606 document table 110 with descriptions of memory addresses */ volatile uint32_t addr = 0x1FFF0000;/**
* Step: Disable RCC, set it to default (after reset) settings * Internal clock, no PLL, etc. */ RCC_DeInit(); __HAL_RCC_SYSCFG_CLK_ENABLE(); /** * Step: Disable systick timer and reset it to default values */ SysTick->CTRL = 0; SysTick->LOAD = 0; SysTick->VAL = 0; /** * Step: Disable all interrupts */ __disable_irq();__DSB();
/**
* Step: Remap system memory to address 0x0000 0000 in address space * For each family registers may be different. * Check reference manual for each family. * * For STM32F4xx, MEMRMP register in SYSCFG is used (bits[1:0]) * For STM32F0xx, CFGR1 register in SYSCFG is used (bits[1:0]) * For others, check family reference manual */ __HAL_SYSCFG_REMAPMEMORY_SYSTEMFLASH(); //Call HAL macro to do this for you/**
* Step: Set jump memory location for system memory * Use address with 4 bytes offset which specifies jump location where program starts */ /* Remap is bot visible at once. Execute some unrelated command! */ __DSB(); __ISB();SysMemBootJump = (void (*)(void)) (*((uint32_t *)(addr + 4)));
/** * Step: Set main stack pointer. * This step must be done last otherwise local variables in this function * don't have proper value since stack pointer is located on different position * * Set direct address location which specifies stack pointer in SRAM location */ __set_MSP(*(uint32_t *)addr);/**
* Step: Actually call our function to jump to set location * This will start system memory execution */SysMemBootJump();
/**
* Step: Connect USB<->UART converter to dedicated USART pins and test * and test with bootloader works with STM32 Flash Loader Demonstrator software */while(1);
}- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-10 10:12 AM
Does it work when you reset with BOOT0=High?
Use a debugger and step into the ROM and get a better understanding about what is actually happening.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-11 7:01 AM
>
volatile uint32_t addr = 0x1FFF0000;
You've forgotten to set bit 0 in the jump address. It is required for the thumb instruction set.
- pa
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-11 8:12 AM
Thank you Clive,
so I tried to put in bootloader mode with BOOT0=HIGH, but it didn't work communication between board and stm32 loader.
I don't know what is happening.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-11 8:40 AM
The loader is going to be highly sensitive to transitions on any of the pins/interfaces where valid activity might be expected. This might take precedence over your signalling on PA9/PA10 later.
Review board design and pin usage.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-11 9:03 AM
>>You've forgotten to set bit 0 in the jump address. It is required for the thumb instruction set.
Yeah, that's not how it works in this context, it is a table full of addresses, not the address it is calling. The address of the ROM Vector Table is correct.
Up vote any posts that you find helpful, it shows what's working..