2017-03-14 11:30 PM
hi,I want use LPTIM1 and select clock source is LSE.
when i enable LSE use code auto-gen from stm32cubemx,but LSERDY can't assert,the external OSC is work normal.
init code like as:
void SystemClock_Config(void)
{ RCC_OscInitTypeDef RCC_OscInitStruct; RCC_ClkInitTypeDef RCC_ClkInitStruct; RCC_PeriphCLKInitTypeDef PeriphClkInit; /**Initializes the CPU, AHB and APB busses clocks */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSE|RCC_OSCILLATORTYPE_MSI; RCC_OscInitStruct.LSEState = RCC_LSE_ON; RCC_OscInitStruct.MSIState = RCC_MSI_ON; RCC_OscInitStruct.MSICalibrationValue = 0; RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /**Initializes the CPU, AHB and APB busses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK) { Error_Handler(); } PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_LPTIM1; PeriphClkInit.Lptim1ClockSelection = RCC_LPTIM1CLKSOURCE_LSE; if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK) { Error_Handler(); } /**Configure LSE Drive Capability */ __HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_HIGH); /**Configure the main internal regulator output voltage */ if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK) { Error_Handler(); } /**Configure the Systick interrupt time */ HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000); /**Configure the Systick */ HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK); /**Enable MSI Auto calibration */ HAL_RCCEx_EnableMSIPLLMode(); /* SysTick_IRQn interrupt configuration */ HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);}what's problem about it?
2017-03-15 3:11 AM
Hi
cai.bai
,Please replace the line below :
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSE|RCC_OSCILLATORTYPE_MSI;
with:
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSE;
This is a reported issue using CubeMX V4.20 and this will be corrected in the coming version.
Sorry for any inconvenience this may have caused.
Khouloud
2017-03-15 7:46 PM
i modify code as you talk,but it can't work.
tickstart = HAL_GetTick();
/* Wait till LSE is ready */
while(READ_BIT(RCC->BDCR, RCC_BDCR_LSERDY) == RESET) { if((HAL_GetTick() - tickstart) > RCC_LSE_TIMEOUT_VALUE) { return HAL_TIMEOUT; } }LSERDY can't assert and then timeout
2017-03-16 1:53 PM
What hardware do you use?
Post the read out content of relevant RCC registers at the moment of timeout.
JW
2017-07-07 11:34 PM
I met the same issue, that LSE can't be ready. any solution for this issue? I'm using L431, 32.768KHz, LSE.