2023-08-03 10:35 PM
Hi,
Im using stm32h7 mcu for my project.Which is an iot product.I need to use low power mode on it i need to wake the mcu using an gpio external interrupt or either by an uart .Device is switch to some mode with a constant current consumption which is a bit higher value.There is only a 20mA difference with run mode on this state.
these are the code which is used to make mcu to low power mode.
ATOMIC_SET_BIT(huart1.Instance->CR3, USART_CR3_WUFIE);
WakeUpEventConfig.WakeUpEvent = UART_WAKEUP_ON_STARTBIT;
HAL_UARTEx_StopModeWakeUpSourceConfig(&huart1, WakeUpEventConfig);
HAL_UARTEx_EnableStopMode(&huart1);
HAL_SuspendTick();
HAL_PWREx_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFE, PWR_D1_DOMAIN);
What should be the reason to have higher current consumption in this mode(im getting around 82mA constant in this mode and getting an increment on run mode to 100mA)?
2023-08-04 2:25 AM
Hello @Error_Code,
Could you share the full configuration of your test: SystemClock_Config(), VOS, flash memory status and all the parameters in this table.

Also, there is an example code using stop mode in the STM32H7CubeFW following this path : STM32Cube\Repository\STM32CubeH7-master\Projects\STM32H747I-DISCO\Examples\PWR
Finally, make sure to set all unused pins to analog as shown in this article : How to minimize the power consumption in low power mode: An example using NUCLEO-F401RE board
Hope that helps!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.