2015-11-10 05:54 AM
Good morning, Someone have try to enable the PVD function, and use
the PA0-WKUP Pin like an Output ?? When i start the PVD functions although i disable the Wake Up pin (PWR_WakeUpPinCmd (DISABLE);) I am not able to control the PA0 like an Output ?? Not function more.... If i disable the PVD the Output PA0 function, normally!, there is some configuration to do ?? thank you