cancel
Showing results for 
Search instead for 
Did you mean: 

Power supply 5v then 3v is it possible ?

julienterrier39
Associate II
Posted on September 10, 2015 at 15:17

Hello,

I use  STM32F429I Discovery-Board to make my project and my question is about power supply available on this board.

I would to know,if it's possible to recover 3V from P2 if  I supply the board by an external dc source  with 5v on P1 ?

I want to use these 3v to supply an RS232 driver to reach the good logic lvl for USART protocol.

thanks.
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on September 10, 2015 at 18:30

There is enough head room in the 3V supply/regulator to use the VDD or 3V on the board to power a MAX3232 chip, or a Bluetooth module, or a GPS receiver. I haven't sat and done the math, but I'd expect you have ~50mA to play with.

If you have higher requirements, the 5V gets you close to 500mA via USB, you can add your own regulators or supplies, common the grounds.

If I had a cellular modem wanting 2A peak, I'd use a completely different supply and regulator arrangement.

The boards can also be run off those USB Lithium battery pack/chargers (juice boxes, or whatever you want to call them, $20 at WalMart).

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
julienterrier39
Associate II
Posted on September 11, 2015 at 14:28

Hi,

thank you for your answer, If I understood it will depend of current's consumption of my elements.

Anyway I will use an external power supply which can provide higher than 1 or 2 A except that this power supply provide 5V. 

I have not made the addition of the current consumed by elements ( µcontroleur, LCD, Max3232,Led etc..) but I am sure that my power supply will be effective.