Question
Input capture in STM32F103RC
Posted on September 01, 2015 at 11:41
Hi
I was trying to configure the input capture in STM32F103RC , and facing issues , The configuration is done as follow I was trying to configure TIM1 CH3 , RCC->APB2ENR |= RCC_APB2ENR_TIM1EN; NVIC_EnableIRQ(TIM1_CC_IRQn); /* reset the Register */ TIM1->CCMR2 |= 0x0001; /* as input capture for TI3 */ TIM1->CCER &= ~0x0200; TIM1->CCER |= 0x0100; TIM1->DIER |= 0x00000008; /* Enabling CC3 Interrupt Enable */ TIM1->PSC = 0x00FF; /* Configuring Prescalar */ TIM1->DMAR = 0x0000; TIM1->ARR = 0x0000; /* Configure the capture control for CH3 */ TIM1->EGR |= 0x00000001; TIM1->CR1 |= 0x0001; Interrupt is not happening and the TIM1_CCR3 register is not getting updated with the Captured value. Am i missing something ,or should we do anything special to capture signal in TIM1_CH3 Help is very much appreciated Thanks & regards kamaraj #timer