cancel
Showing results for 
Search instead for 
Did you mean: 

possible to retrigger Timer3 via ext. TIM3_CH3 or via TIM3_ETR

reinhard2
Associate
Posted on March 04, 2010 at 11:37

possible to retrigger Timer3 via ext. TIM3_CH3 or via TIM3_ETR

1 REPLY 1
lowpowermcu
Associate II
Posted on May 17, 2011 at 13:42

Ni Beraus reinhard,

I have found the following sentence in the reference manual ''The counter and its prescaler can be re-initialized in response to an event on a trigger input.''

It is mentioned in the Timer section.

I hope this hepls you.

Regards,

be low power