OSPI Flashing in IAR EWARM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-02-24 3:54 PM
Hello,
I am working on a project that wants to store pre-built binary files in the OSPI on the STM32L562E-DK. I am using all of the default jumper settings for the board. When I build my project in IAR EWARM 8.50.9 and then try to program the device via the onboard ST-LinkV3, it hangs after programming internal flash. If I disable the OSPI flashing algorithm in the IAR IDE then everything programs correctly.
I can program the hex file built by my project using STM32CubeProgrammer, but I would like to have this work in the IAR IDE itself. Does anyone have an idea of what may be wrong here?
I have attached a simple project that creates some data in the OSPI memory region that can be used to replicate this issue.
Hardware:
STM32L562E-DK
Software:
STM32Cube 6.1
STM32CubeProgrammer 2.6.0
ST-LinkV3 Firmware Version V3J7M3
IAR EWARM 8.50.9
Thanks in advance,
Ian
- Labels:
-
OctoSPI
-
STM32L5 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-03-04 3:41 AM
Hi IFyal.1 ,
If I understand correctly you are facing a problem to program using OSPI only with Ewarm (IAR) but it works fine with CubeProgrammer?
If that is the case I am attaching the patch for EWARM that contains the flasher for OSPI (FlashSTM32L562E-DK_OSPI.out) and it should enable you to program your OSPI on STM32L562E-DK. You just need to install it.
Next step will be to help locate the problem with your code.
I will wait for your feedbacks to see if this works for you.
-Imen