cancel
Showing results for 
Search instead for 
Did you mean: 

Oscillator calculation STM32

Marcel Blindu
Associate II

I want to use a STM32F103, STM32L431, 451 and 471 microcontroller, but i don´t know if the crystal that i selected (ABS07-120-32.768kHz-T and ABMM2-8.000MHZ-E2-T) is valid for this microcontroller.

And another question is how to calcule the load capacitance that a need to put in parralel with crystals.

1 ACCEPTED SOLUTION
2 REPLIES 2
Marcel Blindu
Associate II

Thanks but which values can I suppose for Cin, Cout and Board Strays for STM32F103 and STM32L4 for HSE and LSE using the ecuation 1 in the following datasheet of the abracon "https://abracon.com/uploads/resources/PierceOscillator_Fundamentals.pdf"