cancel
Showing results for 
Search instead for 
Did you mean: 

Only one DMA Channel works

greg_t
Associate II
Posted on October 08, 2010 at 23:46

Only one DMA Channel works

2 REPLIES 2
Posted on May 17, 2011 at 14:10

USART1_TX Uses DMA1_Channel4

USART2_TX Uses DMA1_Channel7

USART3_TX Uses DMA1_Channel1

The RX for each is also different, look at the RM0008 Technical Reference Manual for a diagram and list.

USART1_RX Uses DMA1_Channel5

USART2_RX Uses DMA1_Channel6

USART3_RX Uses DMA1_Channel3
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
greg_t
Associate II
Posted on May 17, 2011 at 14:10

so if I want a DMA channel for USART2_TX and TIM2_CH2 (they both on Channel 7)

I'll have to choose one of them ??