cancel
Showing results for 
Search instead for 
Did you mean: 

on Board STM32H747XIH6 Debugger Solution

Samudra
Associate III

Dear Sir,

We are using the STM32H747 series microcontroller in one of our custom projects.

Could you please recommend a low-cost on-board debugger suitable for this board? Ideally, the debugger should also be compact in size.

Your assistance on this matter is urgently needed and greatly appreciated.

Kind regards,
Samudralankaiah

 

5 REPLIES 5
STTwo-32
ST Employee

Hello @Samudra and welcome to the ST Community.

I suggest you to have a look at the Hw debugger and programmer tools for STM32 products and try to find the suitable debugger solution for you. Personally, I recommend one of the ST-Link V3 or V2 families (genuine products).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

TDK
Super User

Use an ST-Link/V3MINIE and put a standard 14-pin header (Samtec FTSH-107-01-L-DV-K) on your board as the interface.

STLINK-V3MINIE - STLINK-V3 compact in-circuit debugger and programmer for STM32 - STMicroelectronics

 

If you feel a post has answered your question, please click "Accept as Solution".
Samudra
Associate III

Is it possible to get the schematics of the STLINK-V3MINI board to check this? Could you please provide them?

The user manual shows the connector pinout. The schematics are not published.

If you feel a post has answered your question, please click "Accept as Solution".

More importantly, the firmware is not provided.

Perhaps use a Tag-Connect footprint to easily attach an external debug pod.

If you've got a budget to buy IP, perhaps look a Segger J-LINK OB for on-board implementation.  Or CMSIS-DAP

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..