cancel
Showing results for 
Search instead for 
Did you mean: 

NuttX for STM32

spudarnia
Associate II
Posted on December 02, 2009 at 18:01

NuttX for STM32

10 REPLIES 10
16-32micros
Associate III
Posted on May 17, 2011 at 13:26

Dear spudarnia,

Excellent achievement :-) , Many thanks for your contribution to the STM32 communities and sharing with us.

The choice of the STM3210E-EVAL board is perfect, It has many outstanding resources to run Nuttx RTOS and Applications,

I'm very interested to see ''NX Graphics Subsystem'' with the on board 1Mbytes of SRAM and TFT QVGA LCD with a real Framebuffer :-)

Cheers,

STOne-32/

spudarnia
Associate II
Posted on May 17, 2011 at 13:26

Today, October 17, 2009, I released version 0.4.12 of NuttX. This is the 44th release of NuttX. This release is available from Sourceforge:

http://sourceforge.net/projects/nuttx/files/

Detailed release notes and change log are available at this same location.

This release adds basic support for the STMicro STM32, Cortex-M3 MCU. The

specific port is to the STMicro STM3210E-EVAL development board based around the STM32F103ZET6 MCU. Working, Tested Configurations: the NuttX OS test and the NuttShell (NSH).

More about the STM3210E-EVAL:

http://www.st.com/stonline/books/pdf/docs/14220.pdf

More about NX:

http://nuttx.sourceforge.net/NXGraphicsSubsystem.html

More about NSH:

http://nuttx.sourceforge.net/NuttShell.html

It is planned to extend this basic STM32 port for the 0.4.13 NuttX release.

Additional functionality needed for complete STM32 support includes: USB device driver, LCD driver and NuttX graphics (NX) bringup on the development board's display and MicroSD support. An SPI driver and a DMA support was included in this 0.4.12 release, but has not yet been tested.

spudarnia
Associate II
Posted on May 17, 2011 at 13:26

This initial port does not take advantage of many of the features of the STM3210E-EVAL board -- yet. It works only off the internal chip resource. This is good because it should be easily portable to other, lower-end STM32's.

But I will definitely need those additional resources to get the displays working!

jaroslaw2
Associate II
Posted on May 17, 2011 at 13:26

Hi,

Yeah, it would be extremely cool to have OS with graphic library. We can help you test STM32 port.

spudarnia
Associate II
Posted on May 17, 2011 at 13:26

Testing help would be really appreciated. I have a short list of things I want to do before I get started the frame buffer driver. If you want to get the raw changes in real time for testing purposes, you can get them from SourceForge CVS:

cvs -d:pserver:anonymous@nuttx.cvs.sourceforge.net:/cvsroot/nuttx login

cvs -z3 -d:pserver:anonymous@nuttx.cvs.sourceforge.net:/cvsroot/nuttx co -P nuttx

spudarnia
Associate II
Posted on May 17, 2011 at 13:26

Progress toward nuttx-0.4.13 is good. There already is a new SPI driver, and SPI flash driver, and a USB driver (still under test).

During the course of nuttx-0.4.13 debug, I found and fixed several bugs in 0.4.12. Some of these are critical. I have posted patches for the critical bugfixes here:

http://tech.groups.yahoo.com/group/nuttx/files/Patches/

and here:

https://sourceforge.net/tracker/?func=detail&aid=2889476&group_id=189573&atid=929872

spudarnia
Associate II
Posted on May 17, 2011 at 13:26

Today, November 4, 2009, I released version 0.4.13 of NuttX. This is the 45th release of NuttX. This release is available from Sourceforge:

http://sourceforge.net/projects/nuttx/files/

Detailed release notes and change log are available at this same location.

This release extends support for the STMicro STM32, Cortex-M3 MCU by cleaning up many of the bugs in the initial release and by adding USB and serial FLASH drivers.

It is planned to further extend this STM32 port for the 0.4.14 NuttX release by adding a MicroSD driver and verified the USB mass storage device class.

More info about Nuttx:

http://www.nuttx.org

spudarnia
Associate II
Posted on May 17, 2011 at 13:26

Today, December 2, 2009, I released version 4.14 of NuttX. This is the 46th

release of NuttX. This release is available from Sourceforge:

http://sourceforge.net/projects/nuttx/files/

Detailed release notes and change log are available at this same location.

This release further extends support for the STMicro STM32, Cortex-M3 MCU by adding an SDIO interface, adding SDIO-DMA-based MMC/SD support, and resolving several bugs in the DMA and USB driver logic. This new functionality was verified using the NuttX USB mass storage device class.

The USB implementation is functional, but probably not bug-free. If anyone out there has a USB analyzer that can be used to verify the low-level USB

transactions, I'd love to get that data!

If anyone out there will be integrating this USB driver, let me know and I will be more than happy to work with you to resolve any issues.

At this point, I think the NuttX support for the STM32F103ZE chip is complete and, unless someone has some great ideas, I will probably move on to some new NuttX project for the next release.

16-32micros
Associate III
Posted on May 17, 2011 at 13:26

Thank you for the updates :

nuttx-4.14

^^^^^^^^^^

This is the 46th release of NuttX. The release extends the support for the STMicro

STM32 microcontroller. Minimal support for the STM3210E-EVAL development board based

around the STM32F103ZET6 MCU was released in NuttX-0.4.12 and extended in Nuttx-0.4.13

to include initial USB support. This completes the STM32F103ZET6 and adds:

New Generic RTOS Features:

* Added generic support that can be included in any block driver to provide

read-ahead buffering and write buffering for improved driver performance.

* Added a generic worker thread that can used to defer processing from an

interrupt to a task.

* Defined a generic SD/SDIO interface can can be bound to a MMC/SD or SDIO

driver to orovide SDIO support.

* Implemented a an SDIO-based MMC/SD driver using this new SDIO interface

New STM32 Features:

* Add support to configure an STM32 input GPIO to generate an EXTI interrupt.

* Added support for buttons on the STM3210E-EVAL board.

* Implemented an STM32 version of the common the SDIO interface.

* Added a configuration to exercise the STM32 with the USB mass storage

device class example.

This release also corrects some important bugs in the early STM32 release:

* Correct error handling in the mount() logic.

* Fixed several STM32 DMA-related issues. Integrated and debugged STM32 DMA

functionality that was added in 0.4.12.

* Fixed several bugs in the STM32 USB device-side driver.

For USB you should have a USB sniffer to see what hapening...

Cheers,

STOne-32