cancel
Showing results for 
Search instead for 
Did you mean: 

nucleu-h745zi-q rs485 without external module

MGH745
Associate II

Hello
//   nucleu-h745zi-q
I want to use hardware flow control rs485

Previously, i used an external module because there was only rs232 (f103).
** question ** . With this feature, can the module be removed and the microcontroller directly connected to A B receiver?

Mikael
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Pavel A.
Super User

No.

AScha.3
Super User

Hi,

You need to connect a rs485 driver, thats all. And set a UART to 485-mode (thats capable to do this).

Something like DS485M (from Ti) .

look at mouser ... many :

https://www.mouser.de/c/semiconductors/interface-ics/rs-485-interface-ic/?q=rs485&instock=y&sort=pricing

 

If you feel a post has answered your question, please click "Accept as Solution".

Thank you for your answer
I used to run rs485 easily without hardware flow control
I would like to know what difference will be made by adding this feature?

Mikael

The ST-LINK on the NUCLEO does not implement RS232 levels.

RS485 differential pairs need a transceiver, and a control signal to enable the driver. Direction rather than "flow" control

Perhaps RS422 where you have a separate pair for each of transmit and receive signals?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..