2021-01-05 03:18 AM
How can I change the driver to port 4 or how can I install the driver additionally for port 4?
*Edited by moderation: please don't mention your email address publicly on this forum*
Solved! Go to Solution.
2021-01-06 03:32 AM
Thanks for this additonal hint. So in future whenever I need to connect to my external device I first will check if the port managed by windows is still the same. In case it changed I also have to modify my configuration file.
2021-01-05 04:40 AM
The port number is exclusively managed by Windows and cannot (simply) be changed to a specific number. A particular program will usually find the port number(s) automatically or display a list from which it can be selected. Additionally, you can open the Device Manager (as you have already done) and check the VCOM port number of the current device.
Perhaps you could explain what exactly you mean by "only accepts port 4" as the device should only write to or read from a UART connected to the USB MCU?
Regards
/Peter
2021-01-05 09:39 AM
2021-01-05 11:35 PM
You are welcome!
Please note that the port number is assigned dynamically and can even change on a given Windows machine. So it may not be a good idea to set this up in a configuration file.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
/Peter
2021-01-06 03:32 AM
Thanks for this additonal hint. So in future whenever I need to connect to my external device I first will check if the port managed by windows is still the same. In case it changed I also have to modify my configuration file.