cancel
Showing results for 
Search instead for 
Did you mean: 

No write permission in stm32f103 eval board

pradhanrivankar
Associate II
Posted on June 25, 2009 at 10:38

No write permission in stm32f103 eval board

4 REPLIES 4
pradhanrivankar
Associate II
Posted on May 17, 2011 at 13:15

Hello all

I am trying to implement the DOS file system for my SDCARD. but wen i am trying to access some of the SDIO registers, I am getting the no write permission. Can any1 help me out in this. it urgent.

I am using a board STM32f103 with STM firmware lib.

thanks in advance

kutnickg
Associate II
Posted on May 17, 2011 at 13:15

Have you made sure that the switch on the SD card is not in the ''lock'' position? Really obvious suggestion, but it has happened to me before. Especially for SD slots that were moving the lock with some insertions.

pradhanrivankar
Associate II
Posted on May 17, 2011 at 13:15

hi again

the switch is not in the lock position.

thing is the board which i am using is having a SPI interface to the SD card. so if I use the SPI interface , will it work using the SDIO registers.

Plz reply.....

thanks in advance

st3
Associate II
Posted on May 17, 2011 at 13:15

Is it an SDIO card?