cancel
Showing results for 
Search instead for 
Did you mean: 

New STM32 MicroXplorer v2.0

sbmeirow
Associate II
Posted on February 20, 2012 at 00:24

The new STM32 MicroXplorer v2.0 is now ready for download, per an automated email that I received from ST.  The web page says v1.1, but after downloading, the contents says v2.0 and I verified after I installed it.  After you install it, look in the installation directory for the new user manual too.  Version 2.0 supports all STM32 devices as of February 2012, except STM32L15xx(C-D) and STM32L162xx.  This software is freeware package for Windows to help allocate and configure peripheral mapping to STM32 IC pins. 

http://www.st.com/internet/evalboard/product/251717.jsp

I updated this information in the wikipedia article too. 

http://en.wikipedia.org/wiki/STM32&sharpDevelopment_tools

#microxplorer-stm32
1 REPLY 1
raig
Associate
Posted on April 25, 2012 at 14:40

Problem to configure STM32L15x controllers. If I select a pin with the touch controller function all other related pins are also set to TS function and the previous selected function is overwritten. If I try to set a TS pin to one of it's alternate function the hole TS configuration is also relocated.