cancel
Showing results for 
Search instead for 
Did you mean: 

Stm3240g Board Firmware - Port Problem / Question

jlchoobs
Associate II
Posted on April 25, 2012 at 10:39

I am new to and using the Stm3240g Board Firmware.

I have a problem with the Ports though.

With the Usb and SDCard enabled (nothing else attached),

  I can Enable Port PA and PB. 

But when I enable Port PE - then PA and PB become nonfunctional,

 while PE still seems not working either.

Does this make sense ?

(At the same time, Port PD seems to be running as a Timer.)

I am simply toggling Pins once per second.

Enabling PE is enough to cause the problem.

Any Ideas ?

Is there a conflict in how I enable Ports - or a Stm3240g Problem ?
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0