2008-08-03 09:48 PM
New, SMALLER Xtals for STM32...
2011-05-17 03:40 AM
To save even more space, I've been considering using Murata Ceramic resonators (Model CSTCE_G...). It's 3.2mm by 1.3mm and has built-in load capacitors. The only downside I can see is that they are not as accurate as a crystal, but that's not a problem in my application.
Has anyone tried these with the STM32? thanks, Greg2011-05-17 03:40 AM
Many have sought physically smaller 8MHz Crystals. I report/identify two devices below: a) 6x3mm and b) 5x3.2mm. Both are fundamental, smt.
Both currently stock @ Digi-Key: a) 535-9628-1 b) 644-1132-1 Regards,2011-05-17 03:40 AM
Hi Greg.
Yes, we have a prototype board which uses a CSTCE8M00G52A, with a 220R series resistor. So far, it appears to work fine - though we haven't done temperature or EMC tests yet. Steve.