cancel
Showing results for 
Search instead for 
Did you mean: 

Need help for continues Scan ADC of STM32F0

toantq3
Associate II
Posted on October 08, 2012 at 04:23

Dear friends,

I implement continuous scan ADC1 with 8 channels 0,1,4,5,6,7,8,9 I post my code below. There is something, I don't understand that. 

If I configure: 

ADC_InitStructure.ADC_ScanDirection = ADC_ScanDirection_Upward; /*Scan from channel 0 to 18*/

The sequence data outputs of array RegularConvData_Tab[8]:

RegularConvData_Tab[0] of channel 9

RegularConvData_Tab[1] of channel 0

RegularConvData_Tab[2] of channel 1

RegularConvData_Tab[3] of channel 4

RegularConvData_Tab[4] of channel 5

RegularConvData_Tab[5] of channel 6

RegularConvData_Tab[6] of channel 7

RegularConvData_Tab[7] of channel 8

Anybody can help me why output data is not sequential from channel 0-9 for data from 0 to 7.

My code below.

__IO u16 RegularConvData_Tab[ADC1_NUMOFCHANNEL];

/*

*************************************************************************************************************************************

*   LOCAL FUNCTIONS/PROCEDURES *

*************************************************************************************************************************************

*/

void ADC1_Init_GPIOs(void)

{

GPIO_InitTypeDef    GPIO_InitStructure;

/* GPIOA Periph clock enable */

RCC_AHBPeriphClockCmd(ADC1_GPIO_PORT1_CLK, ENABLE);

/* Configure ADC Channel0,1,4,5,6,7 as analog input */

GPIO_InitStructure.GPIO_Pin = ADC1_C1_OUTPUT|ADC1_C1_SENSE|ADC1_C2_OUTPUT|ADC1_C2_SENSE|ADC1_C3_OUTPUT|ADC1_C3_SENSE;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;

GPIO_Init(ADC1_GPIO_PORT1, &GPIO_InitStructure);

/* GPIOB Periph clock enable */

RCC_AHBPeriphClockCmd(ADC1_GPIO_PORT2_CLK, ENABLE);

/* Configure ADC Channe8,9 as analog input */

GPIO_InitStructure.GPIO_Pin = ADC1_C4_OUTPUT|ADC1_C4_SENSE;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;

GPIO_Init(ADC1_GPIO_PORT2, &GPIO_InitStructure);

}

void ADC1_Init_DMA(void)

{

DMA_InitTypeDef   DMA_InitStructure;

/* DMA1 clock enable */

RCC_AHBPeriphClockCmd(ADC1_DMA_CLK , ENABLE);

/* DMA1 Channel1 Config */

DMA_DeInit(ADC1_DMA_CHANNEL);

DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)ADC1_DR_ADDRESS;

DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)RegularConvData_Tab;

DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC;

DMA_InitStructure.DMA_BufferSize = ADC1_NUMOFCHANNEL;

DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;

DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;

DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;

DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;

DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;

DMA_InitStructure.DMA_Priority = DMA_Priority_High;

DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;

DMA_Init(ADC1_DMA_CHANNEL, &DMA_InitStructure);

/* DMA1 Channel1 enable */

DMA_Cmd(ADC1_DMA_CHANNEL, ENABLE);

/* ADC DMA request in circular mode */

ADC_DMARequestModeConfig(ADC1_SCALE, ADC_DMAMode_Circular);

/* Enable ADC_DMA */

ADC_DMACmd(ADC1_SCALE, ENABLE);

}

void ADC1_Init(void)

{

ADC_InitTypeDef     ADC_InitStructure;

/* Initialize ADC structure */

ADC_StructInit(&ADC_InitStructure);

/* Configure the ADC1 in continous mode withe a resolutuion equal to 12 bits  */

ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;

ADC_InitStructure.ADC_ContinuousConvMode = ENABLE; 

ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;

ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; /*[15:12] = 0x00 ; [11:0] = data*/

ADC_InitStructure.ADC_ScanDirection = ADC_ScanDirection_Upward; /*Scan from channel 0 to 18*/ // ADC_ScanDirection_Backward

ADC_Init(ADC1_SCALE, &ADC_InitStructure); 

/* Convert the ADC1 Channel 0,1,4,5,6,7 with  239 Cycles as sampling time */ 

ADC_ChannelConfig(ADC1_SCALE, ADC_Channel_0 , ADC_SampleTime_239_5Cycles);

ADC_ChannelConfig(ADC1_SCALE, ADC_Channel_1 , ADC_SampleTime_239_5Cycles);

ADC_ChannelConfig(ADC1_SCALE, ADC_Channel_4 , ADC_SampleTime_239_5Cycles);

ADC_ChannelConfig(ADC1_SCALE, ADC_Channel_5 , ADC_SampleTime_239_5Cycles);

ADC_ChannelConfig(ADC1_SCALE, ADC_Channel_6 , ADC_SampleTime_239_5Cycles);

ADC_ChannelConfig(ADC1_SCALE, ADC_Channel_7 , ADC_SampleTime_239_5Cycles);

/* Convert the ADC1 Channel 8,9 with  239 Cycles as sampling time */ 

ADC_ChannelConfig(ADC1_SCALE, ADC_Channel_8 , ADC_SampleTime_239_5Cycles);

ADC_ChannelConfig(ADC1_SCALE, ADC_Channel_9 , ADC_SampleTime_239_5Cycles);

/* ADC Calibration */

ADC_GetCalibrationFactor(ADC1_SCALE);

/* Enable ADC1 */

ADC_Cmd(ADC1_SCALE, ENABLE);   

/* Wait the ADCEN falg */

while(!ADC_GetFlagStatus(ADC1_SCALE, ADC_FLAG_ADEN)); 

/* ADC1 regular Software Start Conv */ 

ADC_StartOfConversion(ADC1_SCALE);

}

void ADC_Scale_Init(void)

{

/* ADC1 DeInit */  

ADC_DeInit(ADC1_SCALE);

/* ADC1 Periph clock enable */

RCC_APB2PeriphClockCmd(ADC1_CLK, ENABLE);

ADC1_Init_GPIOs();

ADC1_Init_DMA();

ADC1_Init();

/* Test DMA1 TC flag */

    while((DMA_GetFlagStatus(DMA1_FLAG_TC1)) == RESET ); 

    

    /* Clear DMA TC flag */

    DMA_ClearFlag(DMA1_FLAG_TC1);

}

void main(void)

{

/*ADC*/

ADC_Scale_Init();

while(1)

{

/* Test DMA1 TC flag */

while((DMA_GetFlagStatus(DMA1_FLAG_TC1)) == RESET ); 

/* Clear DMA TC flag */

DMA_ClearFlag(DMA1_FLAG_TC1);

for (cnt = 0; cnt<8; cnt++){

x16_to_str(RegularConvData_Tab[cnt], data_dip);

uart_tx_puts(DEBUG_USART1, uart_tx_get_buf_ptr(DEBUG_USART1), data_dip, 2);

}

}

}
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0