2018-06-12 01:54 AM
I need low power Design MCU. My STM32F334 is Consuming 70 - 72mA. Does is takes 70mA , or something is wrong ?
2018-06-12 02:25 AM
My STM32F334 is Consuming 70 - 72mA. Does is takes 70mA , or something is wrong ?
Actually measured values ?
Under what conditions ?
According to the datasheet, the 70mA are pretty normal at full speed.
I need low power Design MCU.
The F3 family is NOT a low-power design.
Consider the L0 or L4 family instead.
2018-06-12 02:29 AM
can you recommend similar MCU ?
2018-06-12 05:05 AM
I suggest to consider your requirements (peripherals, power consumption, performance), and look at the line-up of the STM32L4xx MCUs.
Or invite ST representatives to make recommendations. I have not use any L4xx yet.